Other Parts Discussed in Thread: SYSBIOS
Hello,
This is my setup:
Software:
- Latest code composer studio which is also updated
- TI RTOS "Task Mutex Example" example
Hardware:
MSP432P401R LaunchPad
What I'm trying to do is visualise the tasks changing via the RTOS analyzer tools.
In this case the Execution Analysis.
I did various searches on the internet and from what I could find it should work when enabled via the mutex.cfg -> Ti-RTOS->Products-> UIA -> LoggingSetup.
I have added loggingsetup to my configuration, added rtos execution analysis for task context and Semaphores. Run-time control of event logging is also on.
Now I have saved the .cfg and rebuild the program successfully. In the debug view I set a breakpoint in each one of the tasks and add the Execution Analysis to the debugging view. It does show up , but nothing ever is displayed in the graph. I can see the tasks change in the RTOS Object View (ROV) but nothing changes in the graph.
I have tried multiple settings and also followed the tutorial in the documentation but ... I must be doing something wrong.
I have tested it with the "Stairstep JTAG StopMode" example and there is seems to work for whatever reason. I have copied the .cfg code and pasted it in the Task example but still no luck.
It would be wonderful if somebody could help me fix this issue. I have used RTOS before on other platforms but this is the first time with TI.
I'm really hoping to get this tool working.
Regards,
Spikee