This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Micron MCP MT29C4G96MAZAPCJA-5IT(LPDDR+NAND) replace part number.

Other Parts Discussed in Thread: DM3730, FLASHTOOL

We always use Micron MCP MT29C4G96MAZAPCJA-5IT(LPDDR+NAND) in our DM3730 system.

But now we can't buy this device,we need the replace part number.

Thanks.

  • Hi user743401,

    You can choose one of the memories from the link:

    =TI%2520%28OMAP%29:1230:0]

    and select Pin ball-168, Pinout TI(OMAP) and Clock rate 200 MHz
    These memory chips are compatible with OMAP3x and DM37x processors but also I suggest you to contact with Micron for availabilities.

    BR
    Tsvetolin Shulev

  • Hi user743401 &Cvetolin Shulev-XID:
    I have got the samilar question,and my CPU is DM3730,and NAND flash: MT29C4G96 ball-168, is a Multi chip packge, of 512MB NAND & 512MB DDR.
    Now,I want to erase the flash by flashtool V1.06,but can not sussess.
    I have changed the dnld_startup_omap3_gp_2g.2nd" to "dnld_startup_omap3_gp_4g.2nd" already.
    The display messages as bellow:
    where others of the configures that I must change?

    please help me,Thank you very much ,in advance.

    -stdout
    -omap 3
    -no_force_package_alignment
    -com 21
    -t 60
    -p CUSTOM_AM37XX_BOARD
    -2
    chip_erase NANDINFO1BITBOOT 0
    Leaving parameter file:temp_script.txt
    @temp_script.txt
    Looking for device (omap com21)
    Please turn off device, then turn it on again
    Awaiting ASIC id
    AsicId items 04
    AsicId id 01 05 01 36 30 07 07
    AsicId secure_mode 13 02 01 00
    AsicId public_id 12 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    AsicId root_key_hash 14 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    Searching 2nd for: CUSTOM_AM37XX_BOARD 363007 07 GP
    Loading second file Targets\2nd-Downloaders\dnld_startup_omap3_gp_4g.2nd
    Entering parameter file:omapflash2nd.txt at line: 11
    -pheriphalboot_reopen
    Reading board configuration file Targets\Configurations\configuration_custom_am37xx.txt
    Reading definition file .\targets\definitions\definitions_omap3.txt
    -board_config Targets\Configurations\configuration_custom_am37xx.txt
    Leaving parameter file:omapflash2nd.txt
    Sending size of second file (0x00006804 bytes)
    Transferring second file to target (0x6804 bytes)
    Closing boot connection
    Found device (omap com21)
    Waiting for 2nd
    Reception failed - timeout after 60 s during peripheral boot (waiting for 2nd)

    Console program failed, exit code: 2

    please help me,Thank you very much ,in advance.
  • I have got the samilar question,and my CPU is DM3730,NAND flash: MT29C4G96 is a Multi chip packge, of 512MB NAND & 512MB DDR.
          Now,I want to erase the flash by flashtool V1.06,but can not sussess.
          I have changed the dnld_startup_omap3_gp_2g.2nd" to "dnld_startup_omap3_gp_4g.2nd" already.
          The display messages as bellow:
           where others of the configures that I must change?

        please help me,Thank you very much ,in advance.

        -stdout
        -omap 3
        -no_force_package_alignment
        -com 21
        -t 60
        -p CUSTOM_AM37XX_BOARD
        -2
        chip_erase NANDINFO1BITBOOT 0
    Leaving parameter file:temp_script.txt
    @temp_script.txt
    Looking for device (omap com21)
    Please turn off device, then turn it on again
    Awaiting ASIC id
    AsicId items 04
    AsicId id            01 05  01  36 30 07 07
    AsicId secure_mode    13 02  01  00
    AsicId public_id     12 15  01  00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    AsicId root_key_hash    14 15  01  00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    Searching 2nd for: CUSTOM_AM37XX_BOARD 363007 07 GP
    Loading second file Targets\2nd-Downloaders\dnld_startup_omap3_gp_4g.2nd
    Entering parameter file:omapflash2nd.txt at line: 11
        -pheriphalboot_reopen
    Reading board configuration file Targets\Configurations\configuration_custom_am37xx.txt
    Reading definition file .\targets\definitions\definitions_omap3.txt
        -board_config Targets\Configurations\configuration_custom_am37xx.txt
    Leaving parameter file:omapflash2nd.txt
    Sending size of second file (0x00006804 bytes)
    Transferring second file to target (0x6804 bytes)
    Closing boot connection
    Found device (omap com21)
    Waiting for 2nd
    Reception failed - timeout after 60 s during peripheral boot (waiting for 2nd)

    Console program failed, exit code: 2

    please help me,Thank you very much ,in advance.