hi,
We are facing an issue with Ethernet connections on AM335x board.
Both interfaces are connected to one switch with eth0 is 192.168.1.xx and eth1 is 192.168.2.xx.
But after booting the board we are unable to ping from AM335x board to PC.
Here first we need to unplug and plug the eth1 interface Ethernet wire, then only we can ping.
Regards,
Sankar.