This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where to Download SD Card Image for TMDXEVM3358?

Other Parts Discussed in Thread: TMDXEVM3358

Hello,

Sorry if this has been posted somewhere, but I can't seem to find the information anywhere.   I'm a relative newbie and am having a hard time booting up the demo provided in the Evaluation Kit for the AM335x (TMDXEVM3358).  I followed the instructions on the quick start guide, and also checked online for erratas, but when I power on the board nothing displays on the LCD.  Unfortunately I don't have a Serial to USB converter, but I'm assuming something would show up on the LCD?  When I plug in the SD Card into the desktop, I do see the three volumes: boot, rootfs, and start_here.  However, there seems to be a lot of references to BeagleBone and not so much the AM335x EVM.  

I'm wondering if the SD Card that was shipped with the EVM is correct for this TMDXEVM3358 evaluation kit?

If not, where can I download a demo image for the TMDXEVM3358 board?  I want to make sure the board is working and did not come dead-on-arrival.

Thanks,

Frank