Hi,
I am using NHD-5.0-800480TF-ATXI#-CTP on am335x platform. My LCD display is proper and TP have created the ft5x0x i2c node and binded the driver and it is probed properly.
Interface has created as event2 for CTP. when i try to capture the CTP touch points it is not giving any response. Please find the below CTP status.
In hardware INT (gpio3-15) is connected without pull-up, WAKE (gpio1-8) is connected with 10k ohm pull-up resistor.
static struct pinmux_config gpio_captouch_mux[] = {
{"uart0_ctsn.gpio1_8", OMAP_MUX_MODE7 | AM33XX_PIN_OUTPUT},
{"mcasp0_fsx.gpio3_15", OMAP_MUX_MODE7 | AM33XX_PIN_INPUT},
{NULL, 0},
};
-----------------------------------------------------------------------------------
root@am335x-evm:~# evtest /dev/input/event2
Input driver version is 1.0.1
Input device ID: bus 0x0 vendor 0x0 product 0x0 version 0x0
Input device name: "ft5x0x_ts"
Supported events:
Event type 0 (Sync)
Event type 1 (Key)
Event code 330 (Touch)
Event type 3 (Absolute)
Event code 0 (X)
Value 0
Min 0
Max 0
Event code 1 (Y)
Value 0
Min 0
Max 0
Event code 48 (Touch Major)
Value 0
Min 0
Max 255
Event code 50 (Width Major)
Value 0
Min 0
Max 200
Event code 53 (Position X)
Value 0
Min 0
Max 800
Event code 54 (Position Y)
Value 0
Min 0
Max 480
Testing ... (interrupt to exit)
-----------------------------------------------------------------------------------
Please guide me how to make it to work CTP on my platform. Find the booting log for your reference.
Regards,
Anil
Starting kernel ... Uncompressing Linux... done, booting the kernel. [ 0.000000] Linux version 3.2.0 (root@ubuntu) (gcc version 4.6.3 (Ubuntu/Linaro 4.6.3-1ubuntu5) ) #59 Wed Sep 9 11:44:37 IST 2015 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] Machine: am335xevm [ 0.000000] Memory policy: ECC disabled, Data cache writeback [ 0.000000] AM335X ES1.0 (sgx neon ) [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048 [ 0.000000] Kernel command line: console=ttyO0,115200n8 rootfstype=ext3 root=/dev/mmcblk0p2 mem=512M rootwait [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 512MB = 512MB total [ 0.000000] Memory: 512720k/512720k available, 11568k reserved, 0K highmem [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB) [ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB) [ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB) [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB) [ 0.000000] .text : 0xc0008000 - 0xc05bb000 (5836 kB) [ 0.000000] .init : 0xc05bb000 - 0xc0653000 ( 608 kB) [ 0.000000] .data : 0xc0654000 - 0xc06b0b28 ( 371 kB) [ 0.000000] .bss : 0xc06b0b4c - 0xc06dd194 ( 178 kB) [ 0.000000] NR_IRQS:396 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] Total of 128 interrupts on 1 active controller [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz [ 0.000000] omap_dm_timer_switch_src: Switching to HW default clocksource(sys_clkin_ck) for timer1, this may impact timekeeping in low power state [ 0.000000] OMAP clocksource: GPTIMER1 at 24000000 Hz [ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms [ 0.000000] Console: colour dummy device 80x30 [ 0.000166] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.087761] pid_max: default: 32768 minimum: 301 [ 0.087863] Security Framework initialized [ 0.087947] Mount-cache hash table entries: 512 [ 0.088278] CPU: Testing write buffer coherency: ok [ 0.088945] devtmpfs: initialized [ 0.107413] omap_hwmod: gfx: failed to hardreset [ 0.123158] omap_hwmod: pruss: failed to hardreset [ 0.124242] print_constraints: dummy: [ 0.124530] NET: Registered protocol family 16 [ 0.126216] OMAP GPIO hardware version 0.1 [ 0.128024] static void __init am335x_evm_init(void) - ############## EVM_Init [ 0.128217] omap_mux_init: Add partition: #1: core, flags: 0 [ 0.129799] static void __init am335x_evm_i2c_init(void) - ############## i2c_Init [ 0.129979] omap_i2c.1: alias fck already exists [ 0.130706] omap2_mcspi.1: alias fck already exists [ 0.130879] omap2_mcspi.2: alias fck already exists [ 0.131084] edma.0: alias fck already exists [ 0.131099] edma.0: alias fck already exists [ 0.131112] edma.0: alias fck already exists [ 0.150295] bio: create slab <bio-0> at 0 [ 0.152167] SCSI subsystem initialized [ 0.153491] usbcore: registered new interface driver usbfs [ 0.153743] usbcore: registered new interface driver hub [ 0.153907] usbcore: registered new device driver usb [ 0.154037] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3 [ 0.154254] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1 [ 0.167781] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz [ 0.169371] tps65910 1-002d: JTAGREVNUM 0x0 [ 0.171637] print_constraints: VRTC: [ 0.173014] print_constraints: VIO: at 1800 mV [ 0.175240] print_constraints: VDD1: 600 <--> 1500 mV at 1325 mV normal [ 0.177442] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal [ 0.178367] print_constraints: VDD3: 5000 mV [ 0.179705] print_constraints: VDIG1: at 1800 mV [ 0.181062] print_constraints: VDIG2: at 1800 mV [ 0.182404] print_constraints: VPLL: at 1800 mV [ 0.183759] print_constraints: VDAC: at 1800 mV [ 0.185108] print_constraints: VAUX1: at 1800 mV [ 0.186472] print_constraints: VAUX2: at 3300 mV [ 0.187816] print_constraints: VAUX33: at 3300 mV [ 0.189166] print_constraints: VMMC: at 3300 mV [ 0.189565] tps65910 1-002d: No interrupt support, no core IRQ [ 0.190863] Advanced Linux Sound Architecture Driver Version 1.0.24. [ 0.191886] Switching to clocksource gp timer [ 0.205572] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host) [ 0.205736] musb-hdrc musb-hdrc.0: dma type: pio [ 0.206459] musb-hdrc musb-hdrc.0: USB OTG mode controller at e081c000 using PIO, IRQ 18 [ 0.206603] musb-hdrc musb-hdrc.1: dma type: pio [ 0.206921] musb-hdrc musb-hdrc.1: MUSB HDRC host driver [ 0.206986] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1 [ 0.207103] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 0.207114] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 0.207124] usb usb1: Product: MUSB HDRC host driver [ 0.207132] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd [ 0.207139] usb usb1: SerialNumber: musb-hdrc.1 [ 0.207879] hub 1-0:1.0: USB hub found [ 0.207903] hub 1-0:1.0: 1 port detected [ 0.208371] musb-hdrc musb-hdrc.1: USB Host mode controller at e081e800 using PIO, IRQ 19 [ 0.208747] NET: Registered protocol family 2 [ 0.208921] IP route cache hash table entries: 4096 (order: 2, 16384 bytes) [ 0.209190] TCP established hash table entries: 16384 (order: 5, 131072 bytes) [ 0.209404] TCP bind hash table entries: 16384 (order: 4, 65536 bytes) [ 0.209530] TCP: Hash tables configured (established 16384 bind 16384) [ 0.209540] TCP reno registered [ 0.209549] UDP hash table entries: 256 (order: 0, 4096 bytes) [ 0.209566] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes) [ 0.209731] NET: Registered protocol family 1 [ 0.209940] RPC: Registered named UNIX socket transport module. [ 0.209951] RPC: Registered udp transport module. [ 0.209957] RPC: Registered tcp transport module. [ 0.209964] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.210155] NetWinder Floating Point Emulator V0.97 (double precision) [ 0.229706] VFS: Disk quotas dquot_6.5.2 [ 0.229762] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.230919] msgmni has been set to 1001 [ 0.231568] io scheduler noop registered [ 0.231579] io scheduler deadline registered [ 0.231626] io scheduler cfq registered (default) [ 0.232724] usbcore: registered new interface driver udlfb [ 0.321981] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0 [ 0.971525] console [ttyO0] enabled [ 0.975802] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1 [ 0.983641] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2 [ 0.991386] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3 [ 0.999160] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4 [ 1.006932] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5 [ 1.022329] brd: module loaded [ 1.029463] loop: module loaded [ 1.033069] i2c-core: driver [tsl2550] using legacy suspend method [ 1.039530] i2c-core: driver [tsl2550] using legacy resume method [ 1.045975] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.131973] No daughter card found [ 1.135567] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write [ 1.144928] Board name: A33515BB [ 1.148297] Board version: 1.4A [ 1.151574] SKU: SKU#01 [ 1.171922] The board is general purpose EVM in profile 0 [ 1.177563] Found invalid GP EVM revision, falling back to Rev1.1A [ 1.183847] LCD configuration - ############## 0a [ 1.192041] LCD configuration - ############## 0a1 [ 1.200133] LCD configuration - ############## 0a3 [ 1.208309] ##01 - pwm backlight - enable_ecap0 [ 1.213602] LCD configuration - ############## 1 [ 1.221790] LCD configuration - ############## 2 [ 1.229789] da8xx_lcdc.0: alias fck already exists [ 1.235417] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel [ 1.256464] Console: switching to colour frame buffer device 100x30 [ 1.275288] omap-gpmc omap-gpmc: GPMC revision 6.0 [ 1.280311] Registering NAND on CS0 [ 1.284623] omap_i2c.2: alias fck already exists [ 1.291982] usb 1-1: new high-speed USB device number 2 using musb-hdrc [ 1.301960] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz [ 1.308499] tsl2550 2-0039: standard operating mode [ 1.314304] tsl2550 2-0039: support ver. 1.2 enabled [ 1.319889] COMM - static void mmc2_wl12xx_init(int evm_id, int profile) - 00 [ 1.327742] omap_hsmmc.0: alias fck already exists [ 1.333138] omap_hsmmc.2: alias fck already exists [ 1.338480] COMM - static void wl12xx_init(int evm_id, int profile) - 00 [ 1.345698] COMM - static void wl12xx_init(int evm_id, int profile) - 01 [ 1.352900] Configure Bluetooth Enable pin... [ 1.357463] COMM - gp_evm_revision == GP_EVM_REV_IS_1_1A - 00 [ 1.363691] LCD configuration - ############## 0b [ 1.372573] _regulator_get: 2-0018 supply Vdd not found, using dummy regulator [ 1.380215] _regulator_get: 2-0018 supply Vdd_IO not found, using dummy regulator [ 1.408647] lis3lv02d: 8 bits 3DLH sensor found [ 1.443243] usb 1-1: New USB device found, idVendor=04b4, idProduct=6572 [ 1.450253] usb 1-1: New USB device strings: Mfr=0, Product=1, SerialNumber=0 [ 1.457728] usb 1-1: Product: USB2.0 Hub [ 1.462856] hub 1-1:1.0: USB hub found [ 1.467078] hub 1-1:1.0: 4 ports detected [ 1.502238] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0 [ 1.513652] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.520835] omap2-nand driver initializing [ 1.525460] ONFI flash detected [ 1.528861] ONFI param page 0 valid [ 1.532526] NAND device: Manufacturer ID: 0x2c, Chip ID: 0x38 (Micron MT29F8G08ABABAWP) [ 1.540897] chipsize = 1024 MB, writesize = 4096, busw = 0, oobsize = 224, erasesize = 524288 [ 1.549820] >>> chip->ecc.mode = 2, mtd->oobsize = 224 [ 1.555389] Creating 8 MTD partitions on "omap2-nand.0": [ 1.560951] 0x000000000000-0x000000080000 : "SPL" [ 1.567174] 0x000000080000-0x000000100000 : "SPL.backup1" [ 1.574332] 0x000000100000-0x000000180000 : "SPL.backup2" [ 1.581260] 0x000000180000-0x000000200000 : "SPL.backup3" [ 1.588104] 0x000000200000-0x000000300000 : "U-Boot" [ 1.594540] 0x000000300000-0x000000380000 : "U-Boot Env" [ 1.601244] 0x000000380000-0x000000d00000 : "Kernel" [ 1.608440] 0x000000d00000-0x000040000000 : "File System" [ 1.719271] OneNAND driver initializing [ 1.771935] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6 [ 1.778406] davinci_mdio davinci_mdio.0: detected phy mask 7fffffff [ 1.785555] davinci_mdio.0: probed [ 1.789115] davinci_mdio davinci_mdio.0: phy[31]: device 0:1f, driver unknown [ 1.796742] PPP generic driver version 2.4.2 [ 1.801322] usb 1-1.2: new full-speed USB device number 3 using musb-hdrc [ 1.808791] PPP BSD Compression module registered [ 1.813732] PPP Deflate Compression module registered [ 1.819397] PPP MPPE Compression module registered [ 1.824686] usbcore: registered new interface driver zd1201 [ 1.830686] usbcore: registered new interface driver cdc_ether [ 1.836973] usbcore: registered new interface driver cdc_eem [ 1.843117] usbcore: registered new interface driver dm9601 [ 1.848984] cdc_ncm: 04-Aug-2011 [ 1.852512] usbcore: registered new interface driver cdc_ncm [ 1.858430] Initializing USB Mass Storage driver... [ 1.863743] usbcore: registered new interface driver usb-storage [ 1.870021] USB Mass Storage support registered. [ 1.875158] usbcore: registered new interface driver usbserial [ 1.881255] usbserial: USB Serial Driver core [ 1.885931] USB Serial support registered for cp210x [ 1.891262] usbcore: registered new interface driver cp210x [ 1.897099] cp210x: v0.09:Silicon Labs CP210x RS232 serial adaptor driver [ 1.904348] USB Serial support registered for pl2303 [ 1.909760] usbcore: registered new interface driver pl2303 [ 1.915600] pl2303: Prolific PL2303 USB to serial adaptor driver [ 1.922564] mousedev: PS/2 mouse device common for all mice [ 1.929679] usb 1-1.2: New USB device found, idVendor=10c4, idProduct=ea60 [ 1.936900] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 1.944552] usb 1-1.2: Product: CP2102 USB to UART Bridge Controller [ 1.951191] usb 1-1.2: Manufacturer: Silicon Labs [ 1.956114] usb 1-1.2: SerialNumber: 0001 [ 1.960480] input: adp5588-keys as /devices/platform/omap/omap_i2c.1/i2c-1/1-0034/input/input1 [ 1.971254] cp210x 1-1.2:1.0: cp210x converter detected [ 1.981340] adp5588_keys 1-0034: Rev.4 keypad, irq 217 [ 1.987367] ==ft5x0x_ts_init== [ 1.990612] ==ft5x0x_ts_probe= [ 1.993823] ==kzalloc= [ 1.997273] input: ft5x0x_ts as /devices/virtual/input/input2 [ 2.052187] usb 1-1.2: reset full-speed USB device number 3 using musb-hdrc [ 2.062398] [FST] FT55x0x Firmware version = 0x30 [ 2.067319] ==probe over = [ 2.070358] ret=0 [ 2.073149] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0 [ 2.079976] i2c /dev entries driver [ 2.084268] Linux video capture interface: v2.00 [ 2.090347] lm75 2-0048: hwmon1: sensor 'tmp275' [ 2.153084] usb 1-1.2: cp210x converter now attached to ttyUSB0 [ 2.232173] usb 1-1.3: new full-speed USB device number 4 using musb-hdrc [ 2.293432] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec [ 2.304398] cpuidle: using governor ladder [ 2.309171] cpuidle: using governor menu [ 2.313506] sdhci: Secure Digital Host Controller Interface driver [ 2.319961] sdhci: Copyright(c) Pierre Ossman [ 2.330212] usbcore: registered new interface driver usbhid [ 2.336069] usbhid: USB HID core driver [ 2.343520] usb 1-1.3: New USB device found, idVendor=10c4, idProduct=ea60 [ 2.350696] usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [ 2.358337] usb 1-1.3: Product: CP2102 USB to UART Bridge Controller [ 2.364973] usb 1-1.3: Manufacturer: Silicon Labs [ 2.369872] usb 1-1.3: SerialNumber: 0001 [ 2.376112] HMC5843 initialized [ 2.382127] cp210x 1-1.3:1.0: cp210x converter detected [ 2.388051] i2c-core: driver [hmc5843] using legacy suspend method [ 2.394527] i2c-core: driver [hmc5843] using legacy resume method [ 2.401799] usbcore: registered new interface driver snd-usb-audio [ 2.408311] ALSA device list: [ 2.411403] No soundcards found. [ 2.414957] oprofile: hardware counters not available [ 2.420217] oprofile: using timer interrupt. [ 2.424713] nf_conntrack version 0.5.0 (8011 buckets, 32044 max) [ 2.431579] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.437266] TCP cubic registered [ 2.440633] NET: Registered protocol family 17 [ 2.445422] Bridge firewalling registered [ 2.449651] lib80211: common routines for IEEE802.11 drivers [ 2.455618] Registering the dns_resolver key type [ 2.460564] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 2.468570] ThumbEE CPU extension supported. [ 2.473090] mux: Failed to setup hwmod io irq -22 [ 2.478644] Power Management for AM33XX family [ 2.483510] Trying to load am335x-pm-firmware.bin (60 secs timeout) [ 2.490200] Copied the M3 firmware to UMEM [ 2.494514] omap_hwmod: wkup_m3: wkup_m3: hwmod data error: OMAP4 does not support st_shift [ 2.508909] clock: disabling unused clocks to save power [ 2.516731] Detected MACID=68:c9:b:a9:34:f2 [ 2.522661] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800) [ 2.562251] usb 1-1.3: reset full-speed USB device number 4 using musb-hdrc [ 2.571547] mmc0: new high speed SDHC card at address 59b4 [ 2.577992] mmcblk0: mmc0:59b4 SS08G 7.40 GiB [ 2.584608] mmcblk0: p1 p2 [ 2.588781] buzzzz - wl12xx_set_power ON status 00 : 1 [ 2.594192] buzzzz - wl12xx_set_power ON status 01 [ 2.683446] usb 1-1.3: cp210x converter now attached to ttyUSB1 [ 2.709671] buzzzz - wl12xx_set_power ON status 00 : 0 [ 2.715085] buzzzz - wl12xx_set_power ON status 02 [ 3.222295] kjournald starting. Commit interval 5 seconds [ 3.232766] EXT3-fs (mmcblk0p2): using internal journal [ 3.238217] EXT3-fs (mmcblk0p2): recovery complete [ 3.247526] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode [ 3.254775] VFS: Mounted root (ext3 filesystem) on device 179:2. [ 3.261941] Freeing init memory: 608K INIT: version 2.88 booting backlight pwm on Starting udev /etc/rcS.d/S06alignment.sh: line 11: echo: write error: Device or resource busy /etc/rcS.d/S06alignment.sh: line 13: /sys/class/gpio/gpio53/value: No such file or directory /etc/rcS.d/S06alignment.sh: line 14: echo: write error: Invalid argument Error: could not load module /lib/ads1015.ko: No such file or directory Error: Module g_mass_storage is not currently loaded SUCCESSFULLY OPENED Received GPS Packet is: [ 8.426705] lun0: unable to open backing file: /dev/mmcblk0p3 [ 8.432950] g_mass_storage musb-hdrc.0: failed to start g_mass_storage: -2 ERROR: could not insert 'g_mass_storage': Unknown symbol in module, or unknown parameter (see dmesg) Executed command : Hardware Information: FATAL: Module ads1015 not found. Starting Bootlog daemon: bootlogd. ALSA: Restoring mixer settings... /usr/sbin/alsactl: load_state:1686: No soundcards found... Configuring network interfaces... [ 9.456968] PHY 0:00 not found [ 9.460195] PHY 0:01 not found udhcpc (v1.20.2) started testingggggggggggggggggggggg............ File not found. Please use the correct I2C-address or connect the adc-module.You can also try to load/reload the module ads1015 Sending discover... Sending discover... Sending discover... No lease, failing done. Sat Jan 1 00:01:00 UTC 2000 INIT: Entering runlevel: 5 Starting system message bus: dbus. Starting Dropbear SSH server: dropbear. Starting telnet daemon. Performing wifi calibration... Error: Module wl12xx_sdio is not currently loaded [ 19.046105] Disabling lock debugging due to kernel taint [ 19.065917] cfg80211: Calling CRDA to update world regulatory domain [ 19.293040] wl12xx: driver version: ol_R5.SP4.01-2-g1aa2c8e [ 19.298864] wl12xx: compilation time: Sat Jan 10 12:45:07 2015 [ 19.313211] cfg80211: World regulatory domain updated: [ 19.318650] cfg80211: (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp) [ 19.327402] cfg80211: (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 19.335667] cfg80211: (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 19.343929] cfg80211: (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm) [ 19.352191] cfg80211: (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) [ 19.360441] cfg80211: (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm) nvs file /lib/firmware/ti-connectivity/wl1271-nvs.bin. File already exists. Won't overwrite. Starting network benchmark server: netserver. Starting syslogd/klogd: done Starting thttpd. Launching Applications Desktop.. /etc/rc5.d/S40app.sh: line 3: cd: /home/pda/app/launcher: No such file or directory ....Launched.... Starting Lighttpd Web Server: lighttpd. 2000-01-01 00:00:00: (log.c.166) server started date: invalid date '000120000101' / Starting Matrix GUI application. [ 25.374595] gadget: Mass Storage Function, version: 2009/09/11 [ 25.380786] gadget: Number of LUNs=1 [ 25.384666] lun0: LUN: removable file: /dev/mmcblk0p1 [ 25.390059] gadget: Mass Storage Gadget, version: 2009/09/11 [ 25.396067] gadget: userspace failed to provide iSerialNumber [ 25.402170] gadget: g_mass_storage ready [ 25.406366] musb-hdrc musb-hdrc.0: MUSB HDRC host driver [ 25.411955] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2 [ 25.419797] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002 [ 25.426898] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 25.434447] usb usb2: Product: MUSB HDRC host driver [ 25.439620] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd [ 25.445163] usb usb2: SerialNumber: musb-hdrc.0 [ 25.451044] hub 2-0:1.0: USB hub found [ 25.455035] hub 2-0:1.0: 1 port detected /etc/rc5.d/S99demon-process: line 3: bug: command not found the size if 4 File opened successfully through fopen() fread() sucessfuly done the read string is060 the the size of buffer is 4 the number of min read is 48 *************************************************************** *************************************************************** NOTICE: This file system contains the followin GPLv3 packages: binutils-symlinks binutils gdbserver If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove <package> Where <package> is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** ********************************************Z _____ _____ _ _ | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_ | | _| .'| . | . | | __| _| . | | | -_| _| _| |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_| |___| |___| Arago Project http://arago-project.org am335x-evm ttyO0 Arago 2013.05 am335x-evm ttyO0