Hi,
I want work with AM1808, with all software on Nor Flash (ubl , u-boot, linux and file system) . I have rebuilded the Linux with Config option like "processors.wiki.ti.com/.../Filesystem_in_NOR_or_NAND" instruction . The Linux see the NOR Flash but the command erase doesn't work.
this is my output board when linux start with ramdisk fs:
OMAP-L138 initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: NOR
Starting Sergio2 NOR Copy...
CFI Query...passed.
NOR Initialization:
Command Set: Intel
Manufacturer: INTEL
Size: 0x00000008 MB
Valid magicnum, 0x55424CBB, found..
DONE
Jumping to entry point at 0xC1080000.
FLASH: 8 MiB
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 150000000 Hz
Net: Ethernet PHY: GENERIC @ 0x00
DaVinci-EMAC
Hit any key to stop autoboot: 0
U-Boot > tftp uImage
Using DaVinci-EMAC device
TFTP from server 172.16.3.23; our IP address is 172.16.3.1
Filename 'uImage'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
######################
done
Bytes transferred = 5080556 (4d85ec hex)
U-Boot > bootm
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-2.6.37
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5080492 Bytes = 4.8 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Linux version 2.6.37 (smv2@smv2) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #8 PREEMPT Wed Sep 9 10:53:37 CEST 2015
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: DaVinci DA850/OMAP-L138/AM18x EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci da850/omap-l138 variant 0x0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 16256
Kernel command line: console=ttyS2,115200n8 root=/dev/mtdblock0 rw rootwait ip=off
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 64MB = 64MB total
Memory: 54188k/54188k available, 11348k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xff000000 - 0xffe00000 ( 14 MB)
vmalloc : 0xc4800000 - 0xfea00000 ( 930 MB)
lowmem : 0xc0000000 - 0xc4000000 ( 64 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.init : 0xc0008000 - 0xc05db000 (5964 kB)
.text : 0xc05db000 - 0xc0a31000 (4440 kB)
.data : 0xc0a32000 - 0xc0a5c700 ( 170 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptable hierarchical RCU implementation.
RCU-based detection of stalled CPUs is disabled.
Verbose stalled-CPUs detection is disabled.
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 149.50 BogoMIPS (lpj=747520)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
devtmpfs: initialized
DaVinci: 144 gpio irqs
regulator: core version 0.5
regulator: dummy:
NET: Registered protocol family 16
WARNING: both McASP and McBSP are enabled, but they share pins.
Only McASP will work. If you want McBSP support, disable McASP.
WARNING: both McASP and UART1_AFE are enabled, but they share pins.
Disable one of them.
da850_evm_init: eHRPWM module 0 cannot be used since it is being used by MII interface
da850_evm_init: eHRPWM module1 outputA cannot be used since it is being used by LCD
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pca953x 1-0020: interrupt support not compiled in
DA850/OMAP-L138 EVM UI card detected
pca953x 1-0021: interrupt support not compiled in
regulator: VDCDC1: 3200 <--> 3300 mV at 3300 mV
regulator: VDCDC2: 1750 <--> 3300 mV at 3300 mV
regulator: VDCDC3: 950 <--> 1350 mV at 1200 mV
regulator: LDO1: 1800 mV
regulator: LDO2: 1150 <--> 1300 mV at 1200 mV
i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
Advanced Linux Sound Architecture Driver Version 1.0.23.
Bluetooth: Core ver 2.15
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Switching to clocksource timer0_1
musb-hdrc: version 6.0, host, debug=0
musb-hdrc musb-hdrc: dma type: dma-cppi41
Waiting for USB PHY clock good...
musb-hdrc musb-hdrc: MUSB HDRC host driver
musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc: USB Host mode controller at fee00000 using DMA, IRQ 58
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 2048 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
EMAC: MII PHY configured, RMII PHY will not be functional
McBSP:Probed McBSP1
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 105
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found Sharp_LK043T1DG01 panel
Console: switching to colour frame buffer device 60x34
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
console [ttyS2] enabled
brd: module loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x01e18000-0x01e19fff] port 0x100 irq 67
physmap platform flash device: 00800000 at 60000000
physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x008817
Intel/Sharp Extended Query Table at 0x010A
Intel/Sharp Extended Query Table at 0x010A
Intel/Sharp Extended Query Table at 0x010A
Intel/Sharp Extended Query Table at 0x010A
Intel/Sharp Extended Query Table at 0x010A
Using buffer write method
Using auto-unlock on power-up/resume
cfi_cmdset_0001: Erase suspend on write enabled
cmdlinepart partition parsing not available
RedBoot partition parsing not available
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: detected phy mask fffffffe
davinci_mdio.0: probed
davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
console [netcon0] enabled
netconsole: network logging started
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
ohci ohci.0: DA8xx OHCI
ohci ohci.0: new USB bus registered, assigned bus number 2
Waiting for USB PHY clock good...
ohci ohci.0: irq 59, io mem 0x01e25000
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: gpio-keys-polled as /devices/platform/gpio-keys-polled.0/input/input0
input: gpio-keys-polled as /devices/platform/gpio-keys-polled.1/input/input1
ata1: SATA link down (SStatus 0 SControl 300)
input: TPS6507x Touchscreen as /devices/platform/i2c-gpio.1/i2c-1/1-0048/input/input2
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
watchdog watchdog: heartbeat 60 sec
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCILL protocol initialized
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
davinci_mmc davinci_mmc.1: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
1-0018 supply IOVDD not found, using dummy regulator
1-0018 supply DVDD not found, using dummy regulator
1-0018 supply AVDD not found, using dummy regulator
1-0018 supply DRVDD not found, using dummy regulator
asoc: tlv320aic3x-hifi <-> davinci-mcasp.0 mapping ok
ALSA device list:
#0: DA850/OMAP-L138 EVM
nf_conntrack version 0.5.0 (846 buckets, 3384 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
Bluetooth: L2CAP ver 2.15
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO (Voice Link) ver 0.6
Bluetooth: SCO socket layer initialized
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
regulator_init_complete: incomplete constraints, leaving LDO2 on
regulator_init_complete: incomplete constraints, leaving LDO1 on
regulator_init_complete: incomplete constraints, leaving VDCDC3 on
regulator_init_complete: incomplete constraints, leaving VDCDC2 on
regulator_init_complete: incomplete constraints, leaving VDCDC1 on
davinci_emac_probe: using random MAC addr: 0a:98:ee:5d:2a:32
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:33:00 UTC (946686780)
Freeing init memory: 5964K
INIT: version 2.88 booting
Starting udev
<30>udevd[562]: starting version 182
Starting Bootlog daemon: bootlogd.
Populating dev cache
Configuring network interfaces... done.
Mon Feb 16 13:19:00 UTC 2015
INIT: Entering runlevel: 5
Starting syslogd/klogd: done
Impossible to start StarMille!
Stopping Bootlog daemon: bootlogd.
Poky (Yocto Project Reference Distro) 1.5 am180x-evm /dev/ttyS2
am180x-evm login: root
root@am180x-evm:~# cat /proc/mtd
dev: size erasesize name
mtd0: 00800000 00020000 "physmap-flash.0"
root@am180x-evm:~# flash_erase /dev/mtd0 0 1
Erasing 128 Kibyte @ 0 -- 0 % complete
the command flash_erase doesn't return. Why ?
Probably isn't Linux configured well ?
The timing of emif bus is correct because u-boot write and read the Nor Flash correctly.
Can you help me ?
Sergio D'Orazio