Hi, all
The hardware is designed by myself, but the powering parts are copied from taht of APPRO-IPNC.
And i haved measured the output TPS659113, the results are qualified in both timing and rating
And, i verified the following conditions:
1、The powering up sequence is correct, i have measured the sequence pairwise~~
2、The voltage ratings are correct (1.2V 1.5V 1.8V 3.3V are all present)~~~
3、The crystal are working in a correct way (i have measured the waves, both are correct (20MHz & 22.5792MHz))
Nevertheless, i found that, RSTOUTn_WD_OUTn is always 0 (Logic Low) while POR is already deasserted from the state " POR = '0' ".
can anyone explain why should this happen