This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM5517, Program DSP with permanent program after reset

Hello all,

I would like to program my EVM5517 board (I'm programming the dsp), so after reset, it reboots with the program I wrote.

Right now, it reboots with the calendar on the lcd as the example from industry. I think it reboots from dsp ROM. The bootloader doesn't work on Windows 8, so I can just program the dsp RAM of the board, using Code Composer. Then, after reset, I lose my program and I see the example again.

How should I do it to write my EMV5517 so it keeps my program after reset? Can I do it using Code Composer Studio?

Thank you in advance

ip