This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pins of the TMDXLCDK138 kit can not work

Other Parts Discussed in Thread: OMAPL138

 I have two TI's development boards, TMDXLCDK138. I wrote a module to configure the SPI0's CS , SIMO, SOMI, ENA pin as the GPIO pins . one board is normal. But  another board's pins can not get the right logic waves. its  registers seem right. but the pins are  always low, no output waves.

there are two difference i can find:

(1) the bad board before Simulation must press the key of the reset.

(2)on the bad board the D7 is always light but in the right board D7 is not work.

what is the problem of the board?  is it the port of the SPI0 damaged?

  • Hi,
    It seems you are trying to connect DSP without waking up.
    You have to wake up the DSP through gel file since it is OMAPL138, ARM will wakeup first after reset.
    Please make sure that you are following the same procedure for the both boards.
    Also, make sure about the boot mode settings.