This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to get dmseg output as the README.pdf file for C6678 EVM, PCIe demo project?

Hi,

My C6678EVM now can generate message on minicom terminal as the README.pdf on PCIe demo projects. But I cannot get the dmseg output as in the pdf file:

EDMA-interrupt:
[86.781006]
[86.781020]
[86.781021]
[86.781022]
[86.781537]
[86.781550]
[86.781555]
[86.781565]
[86.781568]
[86.781583]
Finding the device....
Found TI device
TI device: vendor=0x104c, dev=0xb005, irq=0x0000000b
Reading the BAR areas....
Enabling the device....
pci 0000:04:00.0: PCI INT A -> GSI 16 (level, low) -> IRQ 16
pci 0000:04:00.0: setting latency timer to 64
Access PCIE application register ....
Registering the irq 11 ...
Allocating consistent memory ...

On another terminal (not minicom),

[  327.266385] Generating interrupt to DSP ...
[  328.062093] irq 16: nobody cared (try booting with the "irqpoll" option)
[  328.062099] CPU: 0 PID: 2399 Comm: insmod Tainted: GF          O 3.13.0-32-generic #57~precise1-Ubuntu
[  328.062102] Hardware name: MSI MS-7696/A75MA-G55 (MS-7696), BIOS V1.6 11/12/2012
[  328.062105]  00000000 00000000 f7409f54 c1680147 f75bf9c0 f7409f74 c10ad1c9 c1873df8
[  328.062113]  00000010 00000000 000000ed f75bf9c0 00000010 f7409f90 c10ad587 c130f22d
[  328.062119]  00000000 f75bf9c0 f75bf9c0 00000000 f7409fd4 c10ab326 00000000 00200046
[  328.062125] Call Trace:
[  328.062134]  [<c1680147>] dump_stack+0x41/0x52
[  328.062140]  [<c10ad1c9>] __report_bad_irq+0x29/0xd0
[  328.062143]  [<c10ad587>] note_interrupt+0x107/0x150
[  328.062148]  [<c130f22d>] ? delay_tsc+0x3d/0x70
[  328.062153]  [<c10ab326>] handle_irq_event_percpu+0xa6/0x1f0
[  328.062157]  [<c10ab4aa>] handle_irq_event+0x3a/0x60
[  328.062160]  [<c10adf60>] ? unmask_irq+0x30/0x30
[  328.062163]  [<c10adfae>] handle_fasteoi_irq+0x4e/0xd0
[  328.062165]  <IRQ>  [<c1693272>] ? do_IRQ+0x42/0xc0
[  328.062172]  [<c1693033>] ? common_interrupt+0x33/0x38
[  328.062185]  [<c130f22d>] ? delay_tsc+0x3d/0x70
[  328.062189]  [<c130f18b>] ? __const_udelay+0x1b/0x20
[  328.062195]  [<f84fa470>] ? init_module+0x2a0/0x3d0 [pciedemo]
[  328.062200]  [<c103ec0b>] ? default_send_IPI_allbutself+0x7b/0x80
[  328.062204]  [<c10c4da8>] ? smp_call_function_many+0x1a8/0x220
[  328.062208]  [<c104e0a0>] ? __cpa_flush_all+0x40/0x40
[  328.062211]  [<c104e0a0>] ? __cpa_flush_all+0x40/0x40
[  328.062215]  [<c104e0c5>] ? __cpa_flush_range+0x25/0x30
[  328.062218]  [<c104d973>] ? cpa_flush_range+0x43/0xc0
[  328.062222]  [<c104f01d>] ? change_page_attr_set_clr+0x23d/0x260
[  328.062227]  [<f84fa1d0>] ? pushData+0x290/0x290 [pciedemo]
[  328.062231]  [<c10021c2>] ? do_one_initcall+0xa2/0xf0
[  328.062234]  [<c104f20f>] ? set_memory_nx+0x5f/0x70
[  328.062240]  [<c16770eb>] ? do_init_module+0x80/0x1c6
[  328.062244]  [<c10ca431>] ? load_module+0x361/0x530
[  328.062248]  [<c10c8040>] ? show_initstate+0x50/0x50
[  328.062253]  [<c10ca6ab>] ? SyS_init_module+0xab/0xf0
[  328.062257]  [<c1185b4d>] ? __fput+0x16d/0x220
[  328.062264]  [<c1692b4d>] ? sysenter_do_call+0x12/0x28
[  328.062266] handlers:
[  328.062271] [<f844bb30>] sdhci_irq [sdhci]
[  328.062276] [<f91347a0>] azx_interrupt [snd_hda_intel]
[  328.062278] Disabling IRQ #16
[  328.258908] DMA write throughput is: 685.16 MB/s
[  328.258917] divide error: 0000 [#1] SMP
[  328.259301] Modules linked in: pciedemo(OF+) ftdi_sio usbserial rfcomm bnep bluetooth snd_hda_codec_hdmi snd_hda_codec_realtek snd_hda_intel snd_hda_codec snd_hwdep snd_pcm snd_seq_midi snd_rawmidi snd_seq_midi_event radeon snd_seq snd_timer snd_seq_device joydev ttm drm_kms_helper drm psmouse i2c_piix4 i2c_algo_bit snd serio_raw soundcore k10temp mac_hid snd_page_alloc ppdev parport_pc lp parport pata_acpi hid_generic usbhid hid usb_storage sdhci_pci ahci sdhci r8169 libahci pata_atiixp mii
[  328.263789] CPU: 0 PID: 2399 Comm: insmod Tainted: GF          O 3.13.0-32-generic #57~precise1-Ubuntu
[  328.264647] Hardware name: MSI MS-7696/A75MA-G55 (MS-7696), BIOS V1.6 11/12/2012
[  328.265328] task: e7818cf0 ti: f74dc000 task.ti: f74dc000
[  328.265825] EIP: 0060:[<f84fa4ee>] EFLAGS: 00010246 CPU: 0
[  328.266330] EIP is at init_module+0x31e/0x3d0 [pciedemo]
[  328.266818] EAX: 003d0900 EBX: 003d0900 ECX: 00000000 EDX: 00000000
[  328.267394] ESI: 00000340 EDI: 00000000 EBP: f74dde74 ESP: f74ddd58
[  328.267970]  DS: 007b ES: 007b FS: 00d8 GS: 00e0 SS: 0068
[  328.268466] CR0: 8005003b CR2: b769ea10 CR3: 2790b000 CR4: 000007f0
[  328.269042] Stack:
[  328.269222]  f84fb2f0 000002ad 00000010 000002ad 00000000 0000004b f7bb6340 b360a5c2
[  328.270008]  0000004b 00000000 00000000 000000fc 00000c00 f74dddb4 00000282 f74ddd9c
[  328.270792]  00000282 c1acf014 00000000 c19f50a0 00000008 f7be5a88 f7be5f3c f74dddc0
[  328.271578] Call Trace:
[  328.271802]  [<c103ec0b>] ? default_send_IPI_allbutself+0x7b/0x80
[  328.272363]  [<c10c4da8>] ? smp_call_function_many+0x1a8/0x220
[  328.272901]  [<c104e0a0>] ? __cpa_flush_all+0x40/0x40
[  328.273365]  [<c104e0a0>] ? __cpa_flush_all+0x40/0x40
[  328.273831]  [<c104e0c5>] ? __cpa_flush_range+0x25/0x30
[  328.274312]  [<c104d973>] ? cpa_flush_range+0x43/0xc0
[  328.274776]  [<c104f01d>] ? change_page_attr_set_clr+0x23d/0x260
[  328.275330]  [<f84fa1d0>] ? pushData+0x290/0x290 [pciedemo]
[  328.275843]  [<c10021c2>] do_one_initcall+0xa2/0xf0
[  328.276291]  [<c104f20f>] ? set_memory_nx+0x5f/0x70
[  328.276741]  [<c16770eb>] do_init_module+0x80/0x1c6
[  328.277190]  [<c10ca431>] load_module+0x361/0x530
[  328.277623]  [<c10c8040>] ? show_initstate+0x50/0x50
[  328.278081]  [<c10ca6ab>] SyS_init_module+0xab/0xf0
[  328.278529]  [<c1185b4d>] ? __fput+0x16d/0x220
[  328.278941]  [<c1692b4d>] sysenter_do_call+0x12/0x28
[  328.279395] Code: 17 c9 8b 0d a0 b7 50 f8 89 d8 2b 0d a8 b7 50 f8 31 d2 69 c9 40 42 0f 00 03 0d a4 b7 50 f8 2b 0d ac b7 50 f8 c7 04 24 f0 b2 4f f8 <f7> f1 89 c3 6b c2 64 31 d2 89 5c 24 04 f7 f1 89 44 24 08 e8 8d
[  328.281718] EIP: [<f84fa4ee>] init_module+0x31e/0x3d0 [pciedemo] SS:ESP 0068:f74ddd58
[  328.671768] ---[ end trace 1230c3174f6e80f4 ]---
[  348.098878] type=1400 audit(1442075097.834:70): apparmor="DENIED" operation="capable" profile="/usr/sbin/cupsd" pid=1042 comm="cupsd" capability=36  capname="block_suspend"
[  512.864726] usb 1-2: new high-speed USB device number 4 using ehci-pci
[  512.997579] usb 1-2: New USB device found, idVendor=0b1e, idProduct=0009
[  512.997592] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[  512.997600] usb 1-2: Product: Blackhawk XDS560v2-USB Mezzanine Emulator
[  512.997607] usb 1-2: Manufacturer: Blackhawk
[  512.997613] usb 1-2: SerialNumber: 08:00:28:32:06:08
[  788.437654] usb 1-2: reset high-speed USB device number 4 using ehci-pci
[  789.557333] usb 1-2: reset high-speed USB device number 4 using ehci-pci

How to get message only relevant to TI C6678EVM PCIe card?

Thanks,