This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does EDMA interrupt project "pcieboot_interrupt" support local reset?



Hi,

For C6678 EVM with MCSDK (/mcsdk_2_01_02_06), helloWorld example project can run (ins/rm module) repeatedly with local reset (=1) defined. But the project "pcieboot_interrupt" cannot unloading/reloading.

After inserting this module, it is found in loading state with "cat /proc/modules" command.

[  142.369140] pcieIntr: module verification failed: signature and/or  required key missing - tainting kernel
[  142.369650] Finding the device....
[  142.369677] Found TI device
[  142.369683] TI device: vendor=0x104c, dev=0xb005, irq=0x00000007
[  142.369687] Reading the BAR areas....
[  142.377422] Enabling the device....
[  142.377501] Access PCIE application register ....
[  142.377503] Registering the irq 7 ...
[  142.377518] Allocating consistent memory ...
[  142.388534] Boot entry address is 0x  82e640
[  142.389242] Total 5 sections, 0xf5e4 bytes of data were written
[  145.441142] EIP is at init_module+0x31d/0x3e0 [pcieIntr]

cat /proc/modules
pcieIntr 82017 1 - Loading 0x00000000 (OF+)

"irqpoll" has been added to file: /etc/default/grub

GRUB_CMDLINE_LINUX_DEFAULT="quiet splash irqpoll"

Can your project "pcieboot_interrupt" reload again?

Thanks,