Other Parts Discussed in Thread: SYSBIOS
I created a test app to use a 64 bit general purpose timer on EVM6678.
XdcConf:
var Timer = xdc.useModule('ti.sysbios.timers.timer64.Timer');
I created a timer in C as follows:
#include <ti/sysbios/timers/timer64/Timer.h>
void CreateTimer()
{
// Create the timer
Timer_Params prms;
xdc_runtime_Types_FreqHz freq;
Timer_Params_init(&prms);
prms.period = 10000;
prms.startMode = Timer_StartMode_USER;
prms.periodType = Timer_PeriodType_COUNTS;
prms.arg = (UArg) this;
m_hdlTimer64 = Timer_create(9, TimerISR, &prms, NULL);
Timer_getFreq(m_hdlTimer64, &freq);
double factor = (double)freq.lo / 200.0e6;
double period = 10240.0 * factor;
unsigned int iPeriod = (unsigned int) floor(period + 0.5);
Timer_setPeriod(m_hdlTimer64, iPeriod);
Timer_start(m_hdlTimer64);
}
volatile g_Ticks=0;
void TimerISR(UArg arg)
{
g_Ticks++;
}
Everything gets created properly except the TGCR register. Every time I run this code, the TGCR register is set to 0. When I go into the debugger and set it to 3, everything works. What is missing in my initialization to get the GPTR set correctly?
Thanks,
Dan