This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ARM SoftwareLeveling fail

Hello,

In one of the Board we tried to do software levelling but failed to generate optimal seed values,

we are unable to Poke in Values to any DDR location,

I have attached the log file for CCS console output after running "DDR3_SlaveRatio_ByteWiseSearch_TI816x.out".

Please help on this issue asap.

Thanks,

Pramod

  • Hello,

    Sorry Log file was not attached to previous post,

    please see attached file.

    Thanks,

    Pramod

    [CortexA8] Enter 0 for DDR Controller 0 & 1 for DDR Controller 1 
    0
    DDR START ADDR=0x80000000
    
    Enter the Seed Read DQS Gate Ratio Value in Hex to search the RD DQS Gate Window
    
    aa
    
    Enter the Seed Read DQS Ratio Value in Hex to search the RD DQS Ratio Window
    
    40
    
    Enter the Seed Write DQS Ratio Value in Hex to search the Write DQS Ratio Window
    
    9
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    RD DQS GATE RATIO MINIMUM VALUE DIDN'T CONVERGE 
    *********************************************************
    	Byte level Slave Ratio Search Program Values  
    *********************************************************
    			BYTE0	BYTE1	BYTE2	BYTE3
    *********************************************************
    Read DQS MAX		0 	0 	0 	0
    Read DQS MIN		0 	0 	0 	0
    Read DQS OPT		0 	0 	0 	0
    *********************************************************
    Read DQS GATE MAX	0	0 	0 	0
    Read DQS GATE MIN	0	0 	0 	0
    Read DQS GATE OPT	0	0 	0 	0
    *********************************************************
    Write DQS MAX	0 	0 	0 	0
    Write DQS MIN   	0 	0 	0 	0
    Write DQS OPT	0 	0 	0 	0
    
    ===== END OF TEST =====
    

  • Hello Pavel,

    Thanks for the reply,

    I am able to Run .Gel file and initialize the DDR Hardware, I Probed at DDR[0]_CLK[0] and DDR[0]_CLK[1] pins,

    Was able to make difference in P - P Voltage swing between ARM Booting Board and this Board on Clock pin of DDR,

    DDR Clock Level,

    ARM Booting Board - 200mVp-p,

    ARM Non Booting Board - 100mVp-p

     

  • Hello Pavel,

    Thanks for the reply,

    I am able to Run .Gel file and initialize the DDR Hardware, I Probed at DDR[0]_CLK[0] and DDR[0]_CLK[1] pins,

    Was able to make difference in P - P Voltage swing between ARM Booting Board and this Board on Clock pin of DDR,

    DDR Clock Level,

    ARM Booting Board - 200mVp-p,

    ARM Non Booting Board - 100mVp-p

    Thanks

    Pramod