Other Parts Discussed in Thread: TCI6638K2K
Hi,
As Bit rate Co-processor (BCP) support two interface for input/output Multi core Navigator and DIO sub-module. In pdk , given example project is based on Multi core Navigator (PKTDMA) .
1. is there any project for BCP, based on Standalone DIO Sub-module as input/output interface???
2. If we use Standalone DIO Sub-module interface to BCP instead Multi core Navigator interface.
is there any impact on DOWN LINK processing with respect to Rel99 and WCDMA HSDPA processing?
Because as per BCP User Guide page no 205, paragraph 3 last line...........
"This mode of using DIO can be used with any of the BCP submodules but is intended to read the transport channel data for the second stage of R99 downlink processing (radio frame processing)"
3. At present we are planing to use the BCP ENCODER Sub-module only. May be in future, we will use all other BCP Sub modules for complete WCDMA down link processing.
So in net ->want to know the points to take care, if we use Standalone DIO Sub-module interface to BCP instead Multi core Navigator interface.
-> is there any BCP example project with Standalone DIO Sub-module interface.
I have gone through BCP user guide (i.e sprugz1a) Silicon Errata for "BCP DIO Reading From DDR Memory Issue" .I have searched a lot over e2e forum discussion/query for BCP example project with Standalone DIO Sub-module interface to BCP and information regarding it. But not able to get example project and much detail.
We are using C6000 TCI6638K2K device , pdk_keystone2_3_01_01_04, CCS5.5.0.00077 , mcsdk_bios_3_01_01_04, XdcTool Version : 3.25.6.96 and emulator connection Texas Instrument XDS2xx USB Emulator.
Thanks & Regards
Parveen