Hi,
When I run a GPIO project for Tiva-C 1294 LaunchPad, it is found that the SysMin does not show the message as expected. After step through the code, I see the message before System_flush(). The message in the buffer is cleared after System_flush().
Here is the code:
int main(void)
{
/* Call board init functions */
Board_initGeneral();
Board_initGPIO();
Board_initUART();
/* Turn on user LED */
GPIO_write(Board_LED0, Board_LED_ON);
System_printf("Starting the GPIO Interrupt example\nSystem provider is set"
" to SysMin. Halt the target to view any SysMin contents in"
" ROV.\n");
/* SysMin will only print to the console when you call flush or exit */
System_flush();
/* install Button callback */
GPIO_setCallback(Board_BUTTON0, gpioButtonFxn0);
/* Enable interrupts */
GPIO_enableInt(Board_BUTTON0);
/*
* If more than one input pin is available for your device, interrupts
* will be enabled on Board_BUTTON1.
*/
if (Board_BUTTON0 != Board_BUTTON1) {
/* install Button callback */
GPIO_setCallback(Board_BUTTON1, gpioButtonFxn1);
GPIO_enableInt(Board_BUTTON1);
}
/* Start BIOS */
BIOS_start();
return (0);
}
There is some posts on the forum, such as the below link. All are contrary to what my example shows. Is there something different from those old threads and the comments before the System_flush() line.
/* SysMin will only print to the console when you call flush or exit */
The config file is also attached for your reference.3771.gpiointerrupt.cfg