This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Memory leak issue with NDK Reboot

Hi,

We have an issue in restarting NDK.
We see memory leak with NDK reboot,the memory allocation fails with few NDK restarts.

We are using a bit old versions of the NDK.

NDK 2.0
CCS v3.3.81.6
BIOS 5.33.06
CGT v6.0.19

In our application we need to restart the communication(NDK) in order to get rid of a communication error.

Currently we are using NC_NetStop(1) to restart NDK and it is working properly.

But the problem is when we restart few times (around 5 times) the NDK stops working,
and we found that the problem occurs with the memory allocation for PBM_alloc.
When we checked the address of PBM_alloc/PBM_free, we found there is a memory leak.

I would like to know what could be the proper procedure to restart the NDK
do we need to do anything else before executing NDK_NetStop(1)?

Best Regards
kummi