Hello,
I want to use C6678 with 5Gbps PCIe using 100MHz PCIECLK. Could I realize this use case?
I see the following document. Does this description mean that 2.5GHz PLL output frequency can realize 5Gbps?
Keystone PCIe UG (SPRUGS6D): 2.3.3 Reference Clock Multiplication
"The targeted PLL output frequency (line rate) is 2.5 GHz in both PCIe Gen1 and Gen2 modes."
I also see the following document. I see a description of line rate for 5Gpbs (5000Mbps). But I can't see a description of line rate for 5Gpbs by 100MHz reference clock.
Hardware Design Guide for KeyStone I Devices (SPRABI2C): 6.6.2 Configuration of PCIe
And I'm not sure about rate scale. Please give me some advice.
Regards,
Kazu