Hi,
I'm having a problem with C6670.
When I load my program via CCS, execution(running) starts automatically sometimes.
Then following message will displayed at console.
*************************************************************
C66xx_0: Power Failure on Target CPU
C66xx_0: Failed to remove the debug state from the target before disconnecting.
There may still be breakpoint op-codes embedded in program memory.
It is recommended that you reset the emulator before you connect and reload your program before you continue debugging **************************************************************
Sometimes it will stop at main() which is usual but sometime it keep running.
What will cause this problem?
best regards,
g.f.