Hi,
I am trying to understand the FFT Coprocessor on 6670(EVM). So I started with the FFTC simple test example project from the below path.
C:\ti\pdk_C6670_1_1_2_6\packages\ti\drv\exampleProjects\FFTC_Simple_testProject
Procedure :
1. EVM is in No Boot mode.
2. Compiled the project and loaded the same output file to all the cores.
3. Grouped all the cores and executed the group.
I don't see any output on the console and the program seems to be running forever. I did not do any modifications to the example code. Is there any specific procedure I need to follow to execute this project ? Can I get some help in executing this project ?
Thanks
Hari