I'm trying to determine if two options cause any issues.
1st Option: MMC1 using subset of GPMC
I'm using the GPMC attached to an FPGA, and only really need addresses up to A7.
Can I use the MMC1 and GPMC up to A7?
2nd Option: Subset of MMC0
Can I use only data pins of MMC0 up to Dat3 and still use the GMII1 interface?
Ether one of these results in "conflicts" using the PinMux tool, but I'm wondering if either are ok anyway since I don't actually"need" the other pins.