This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 H.264 Encoder with multiple cores

Hello,

We are able to run H264 encoder version 01.00.01.04 with 4 cores. With 5 cores we are seeing some issues when we try to stream the encoded packets.

But when I try to use 6 cores, core 0 is always getting stuck at

                      RMAN_assignResources((IALG_Handle)handle,resFxns, scratchId);  

while other cores go past RMAN_assignResources. I verified handle is not null and am using scratchId = -1 ( FC version is 3.23.02.16)

I tried scratchId = 0 along with cfg settings as mentioned in the below link, but that didn't work.

http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/p/293191/1023645

What could be the reasons for this behavior and how can I debug this further?

Can I get framework components CCS project so I can rebuild FC with debug as I need to find where it hangs in RMAN_assignResources ? 

Thanks
Anish 
Signalogic