This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dwc3.0.auto : NULL pointer dereference , kernel panic - Kernel V3.14.43



i am facing null pointer dereference and kernel panic  in kernel 3.14.43 version during binding ConfigFS functions to UDC driver (dwc3.0.auto) i .e during  $ echo "dwc3.0.auto"   >  /sys/kernel/config/usb_gadget/g1/UDC.


my setup is as follows


DEVICE SETUP  : acts as Gadget. x86-Architecture development Board  booted with kernel 3.14.43

HOST setup   : Minnow MAX board , Acts as  HOST  booted with 3.14.43 kernel.

Both  DEVICE & HOST  are interconnected with USB B-type to A-type connector.

 

the following error occurs if   XHCI controller is enabled at in MINNOW MAX board and NO kernel panic if disable XHCI and enable EHCI controller.

 Please help if any body as idea why this problem occurs .  thanks i advance.

 

Regards

Praveen 

[  302.181188] configfs-gadget gadget: high-speed config #1: c
[  355.759581] BUG: unable to handle kernel NULL pointer dereference at   (null)
[  355.759615] IP: [<  (null)>]   (null)
[  355.759635] *pde = 00000000
[  355.759640] Oops: 0010 [#1] SMP
[  355.759646] Modules linked in: usb_f_ncm u_ether libcomposite fuse ebtable_nat nf_conntrack_netbios_ns nf_conntrack_broadcast ipt_MASQUERADE ip6table_mangle iptable_nat nf_nat_ipv4 nf_nat iptable_mangle xt_conntrack ebtable_filter ebtables be2iscsi iscsi_boot_sysfs bnx2i cnic uio cxgb4i cxgb4 cxgb3i cxgb3 libcxgbi ib_iser rdma_cm iw_cm ib_cm ib_sa ib_mad ib_core ib_addr iscsi_tcp libiscsi_tcp libiscsi scsi_transport_iscsi vhost_net vhost macvtap macvlan kvm_intel kvm i2c_hid joydev i2c_designware_platform iTCO_wdt i2c_designware_pci pcspkr serio_raw iTCO_vendor_support lpc_ich video i2c_designware_core iosf_mbi
[  355.759720] CPU: 2 PID: 2057 Comm: irq/22-dwc3 Not tainted 3.14.48-07127015+ #1
[  355.759725] Hardware name: Intel Corp. VALLEYVIEW D0 PLATFORM/NOTEBOOK, BIOS BYTICRB1.86C.0092.R32.1410021707 10/02/2014
[  355.759729] task: e75ec4c0 ti: e770e000 task.ti: e770e000
[  355.759734] EIP: 0060:[<00000000>] EFLAGS: 00010097 CPU: 2
[  355.759739] EIP is at 0x0
[  355.759743] EAX: f40c2d64 EBX: f40c2c20 ECX: 0000030c EDX: e75c4990
[  355.759747] ESI: ebe4cb80 EDI: f40d1494 EBP: e770ff0c ESP: e770fec4
[  355.759751]  DS: 007b ES: 007b FS: 00d8 GS: 0000 SS: 0068
[  355.759755] CR0: 8005003b CR2: 00000000 CR3: 01174000 CR4: 001007d0
[  355.759758] Stack:
[  355.759761]  c08eda0a 00000001 e770fee4 f40b0840 ebe4cb80 ebe4cb80 f40c2d64 0000030c
[  355.759774]  00000292 00000004 00000000 00000000 00000308 c046c762 00000401 ebe4cb80
[  355.759786]  ebe4cb80 f40b0840 e770ff20 c047daac f40b0840 ebe4cb80 e75ec4c0 e770ff50
[  355.759798] Call Trace:
[  355.759809]  [<c08eda0a>] ? dwc3_thread_interrupt+0x449/0x5b9
[  355.759818]  [<c046c762>] ? __wake_up+0x40/0x47
[  355.759825]  [<c047daac>] irq_thread_fn+0x18/0x2a
[  355.759831]  [<c047e221>] irq_thread+0x81/0x11f
[  355.759837]  [<c047da94>] ? irq_finalize_oneshot+0x7c/0x7c
[  355.759843]  [<c047e2bf>] ? irq_thread+0x11f/0x11f
[  355.759849]  [<c047e1a0>] ? wake_threads_waitq+0x31/0x31
[  355.759856]  [<c0454997>] kthread+0x87/0x8c
[  355.759865]  [<c0bef237>] ret_from_kernel_thread+0x1b/0x28
[  355.759871]  [<c0454910>] ? __kthread_parkme+0x55/0x55
[  355.759875] Code:  Bad EIP value.
[  355.759881] EIP: [<00000000>] 0x0 SS:ESP 0068:e770fec4
[  355.759889] CR2: 0000000000000000
[  355.759894] ---[ end trace 4e43c7c5a826aa49 ]---
[  355.759899] BUG: sleeping function called from invalid context at kernel/locking/rwsem.c:20
[  355.759903] in_atomic(): 1, irqs_disabled(): 1, pid: 2057, name: irq/22-dwc3
[  355.759909] CPU: 2 PID: 2057 Comm: irq/22-dwc3 Tainted: G      D      3.14.48-07127015+ #1
[  355.759913] Hardware name: Intel Corp. VALLEYVIEW D0 PLATFORM/NOTEBOOK, BIOS BYTICRB1.86C.0092.R32.1410021707 10/02/2014
[  355.759916]  00000000 00000000 e770fccc c0be028e e75ec880 e770fcf4 c045ca92 c0e9f750
[  355.759928]  00000001 00000001 00000809 e75ec880 e75e0d70 00000009 00000046 e770fd00
[  355.759940]  c0be851d e75ec4c0 e770fd18 c0449f1b ffffffff 00000000 e75ec4c0 00000009
[  355.759952] Call Trace:
[  355.759959]  [<c0be028e>] dump_stack+0x48/0x60
[  355.759967]  [<c045ca92>] __might_sleep+0xdd/0xe5
[  355.759974]  [<c0be851d>] down_read+0x1c/0x30
[  355.759981]  [<c0449f1b>] exit_signals+0x1f/0x104
[  355.759987]  [<c043e5c7>] do_exit+0xec/0x7de
[  355.759994]  [<c0bdb429>] ? printk+0x4d/0x4f
[  355.760001]  [<c043c951>] ? print_oops_end_marker+0x2f/0x31
[  355.760008]  [<c0bea294>] oops_end+0x98/0x9e
[  355.760014]  [<c0bda845>] no_context+0x17c/0x184
[  355.760021]  [<c0bda96f>] __bad_area_nosemaphore+0x122/0x12a
[  355.760029]  [<c040747b>] ? native_sched_clock+0x46/0x4b
[  355.760036]  [<c0bda98e>] bad_area_nosemaphore+0x17/0x19
[  355.760042]  [<c0bec12a>] __do_page_fault+0x32c/0x3ac
[  355.760049]  [<c06fae84>] ? __delay+0xe/0x10
[  355.760056]  [<c06f597b>] ? plist_del+0x41/0x4c
[  355.760062]  [<c04690e4>] ? dequeue_pushable_task+0x1f/0x45
[  355.760068]  [<c046a46e>] ? dequeue_task_rt+0x27/0x2e
[  355.760075]  [<c045dccc>] ? dequeue_task+0x93/0x9b
[  355.760081]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.760087]  [<c0bec1b5>] do_page_fault+0xb/0xd
[  355.760093]  [<c0be9bca>] error_code+0x5a/0x60
[  355.760099]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.760106]  [<c08eda0a>] ? dwc3_thread_interrupt+0x449/0x5b9
[  355.760112]  [<c046c762>] ? __wake_up+0x40/0x47
[  355.760118]  [<c047daac>] irq_thread_fn+0x18/0x2a
[  355.760124]  [<c047e221>] irq_thread+0x81/0x11f
[  355.760130]  [<c047da94>] ? irq_finalize_oneshot+0x7c/0x7c
[  355.760136]  [<c047e2bf>] ? irq_thread+0x11f/0x11f
[  355.760142]  [<c047e1a0>] ? wake_threads_waitq+0x31/0x31
[  355.760148]  [<c0454997>] kthread+0x87/0x8c
[  355.760155]  [<c0bef237>] ret_from_kernel_thread+0x1b/0x28
[  355.760161]  [<c0454910>] ? __kthread_parkme+0x55/0x55
[  355.760167] note: irq/22-dwc3[2057] exited with preempt_count 1
[  355.760192] BUG: unable to handle kernel paging request at ffffffe0
[  355.760197] IP: [<c0454e4b>] kthread_data+0xf/0x13
[  355.760203] *pde = 0128f067 *pte = 00000000
[  355.760209] Oops: 0000 [#2] SMP
[  355.760213] Modules linked in: usb_f_ncm u_ether libcomposite fuse ebtable_nat nf_conntrack_netbios_ns nf_conntrack_broadcast ipt_MASQUERADE ip6table_mangle iptable_nat nf_nat_ipv4 nf_nat iptable_mangle xt_conntrack ebtable_filter ebtables be2iscsi iscsi_boot_sysfs bnx2i cnic uio cxgb4i cxgb4 cxgb3i cxgb3 libcxgbi ib_iser rdma_cm iw_cm ib_cm ib_sa ib_mad ib_core ib_addr iscsi_tcp libiscsi_tcp libiscsi scsi_transport_iscsi vhost_net vhost macvtap macvlan kvm_intel kvm i2c_hid joydev i2c_designware_platform iTCO_wdt i2c_designware_pci pcspkr serio_raw iTCO_vendor_support lpc_ich video i2c_designware_core iosf_mbi
[  355.760285] CPU: 2 PID: 2057 Comm: irq/22-dwc3 Tainted: G      D      3.14.48-07127015+ #1
[  355.760289] Hardware name: Intel Corp. VALLEYVIEW D0 PLATFORM/NOTEBOOK, BIOS BYTICRB1.86C.0092.R32.1410021707 10/02/2014
[  355.760293] task: e75ec4c0 ti: e770e000 task.ti: e770e000
[  355.760297] EIP: 0060:[<c0454e4b>] EFLAGS: 00010202 CPU: 2
[  355.760302] EIP is at kthread_data+0xf/0x13
[  355.760305] EAX: 00000000 EBX: e75ec4c0 ECX: e770ff3c EDX: e770ff3c
[  355.760309] ESI: e75ec4c0 EDI: 00000046 EBP: e770fd08 ESP: e770fcec
[  355.760313]  DS: 007b ES: 007b FS: 00d8 GS: 0000 SS: 0068
[  355.760317] CR0: 8005003b CR2: ffffffe0 CR3: 01174000 CR4: 001007d0
[  355.760320] Stack:
[  355.760322]  c047e313 e75ec4c0 e75ec4c0 00000000 e770fd10 e75ec4c0 00000000 e770fd18
[  355.760335]  c0452926 e75ec4c0 e75ec4c0 e770fd74 c043e878 c0e9a968 e75ec880 00000809
[  355.760347]  00000001 e770fe88 00000046 e770fd58 e75ec9a4 00000000 00000004 00000001
[  355.760359] Call Trace:
[  355.760365]  [<c047e313>] ? irq_thread_dtor+0x54/0x9e
[  355.760373]  [<c0452926>] task_work_run+0x68/0x8a
[  355.760379]  [<c043e878>] do_exit+0x39d/0x7de
[  355.760386]  [<c043c951>] ? print_oops_end_marker+0x2f/0x31
[  355.760393]  [<c0bea294>] oops_end+0x98/0x9e
[  355.760399]  [<c0bda845>] no_context+0x17c/0x184
[  355.760406]  [<c0bda96f>] __bad_area_nosemaphore+0x122/0x12a
[  355.760413]  [<c040747b>] ? native_sched_clock+0x46/0x4b
[  355.760419]  [<c0bda98e>] bad_area_nosemaphore+0x17/0x19
[  355.760426]  [<c0bec12a>] __do_page_fault+0x32c/0x3ac
[  355.760432]  [<c06fae84>] ? __delay+0xe/0x10
[  355.760438]  [<c06f597b>] ? plist_del+0x41/0x4c
[  355.760444]  [<c04690e4>] ? dequeue_pushable_task+0x1f/0x45
[  355.760450]  [<c046a46e>] ? dequeue_task_rt+0x27/0x2e
[  355.760457]  [<c045dccc>] ? dequeue_task+0x93/0x9b
[  355.760463]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.760469]  [<c0bec1b5>] do_page_fault+0xb/0xd
[  355.760475]  [<c0be9bca>] error_code+0x5a/0x60
[  355.760482]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.760488]  [<c08eda0a>] ? dwc3_thread_interrupt+0x449/0x5b9
[  355.760495]  [<c046c762>] ? __wake_up+0x40/0x47
[  355.760501]  [<c047daac>] irq_thread_fn+0x18/0x2a
[  355.760507]  [<c047e221>] irq_thread+0x81/0x11f
[  355.760513]  [<c047da94>] ? irq_finalize_oneshot+0x7c/0x7c
[  355.760519]  [<c047e2bf>] ? irq_thread+0x11f/0x11f
[  355.760525]  [<c047e1a0>] ? wake_threads_waitq+0x31/0x31
[  355.760531]  [<c0454997>] kthread+0x87/0x8c
[  355.760538]  [<c0bef237>] ret_from_kernel_thread+0x1b/0x28
[  355.760544]  [<c0454910>] ? __kthread_parkme+0x55/0x55
[  355.760548] Code: 3e 8d 74 26 00 64 a1 a4 56 16 c1 8b 80 48 03 00 00 5d 8b 40 d8 c1 e8 02 83 e0 01 c3 55 89 e5 3e 8d 74 26 00 8b 80 48 03 00 00 5d <8b> 40 e0 c3 55 89 e5 52 3e 8d 74 26 00 b9 04 00 00 00 8b 90 48
[  355.760617] EIP: [<c0454e4b>] kthread_data+0xf/0x13 SS:ESP 0068:e770fcec
[  355.760624] CR2: 00000000ffffffe0
[  355.760628] ---[ end trace 4e43c7c5a826aa4a ]---
[  355.760631] Fixing recursive fault but reboot is needed!
[  355.760635] BUG: scheduling while atomic: irq/22-dwc3/2057/0x00000002
[  355.760638] Modules linked in: usb_f_ncm u_ether libcomposite fuse ebtable_nat nf_conntrack_netbios_ns nf_conntrack_broadcast ipt_MASQUERADE ip6table_mangle iptable_nat nf_nat_ipv4 nf_nat iptable_mangle xt_conntrack ebtable_filter ebtables be2iscsi iscsi_boot_sysfs bnx2i cnic uio cxgb4i cxgb4 cxgb3i cxgb3 libcxgbi ib_iser rdma_cm iw_cm ib_cm ib_sa ib_mad ib_core ib_addr iscsi_tcp libiscsi_tcp libiscsi scsi_transport_iscsi vhost_net vhost macvtap macvlan kvm_intel kvm i2c_hid joydev i2c_designware_platform iTCO_wdt i2c_designware_pci pcspkr serio_raw iTCO_vendor_support lpc_ich video i2c_designware_core iosf_mbi
[  355.760710] CPU: 2 PID: 2057 Comm: irq/22-dwc3 Tainted: G      D      3.14.48-07127015+ #1
[  355.760713] Hardware name: Intel Corp. VALLEYVIEW D0 PLATFORM/NOTEBOOK, BIOS BYTICRB1.86C.0092.R32.1410021707 10/02/2014
[  355.760716]  00000000 00000000 e770fa98 c0be028e e75ec4c0 e770fab0 c0bdb030 c0e9f5b7
[  355.760728]  e75ec880 00000809 00000002 e770fb38 c0be6208 c11c74a8 00000400 00015e10
[  355.760740]  0170fad4 00000464 c116b600 c116b600 0000002c 00000001 00000002 e770fb20
[  355.760752] Call Trace:
[  355.760759]  [<c0be028e>] dump_stack+0x48/0x60
[  355.760765]  [<c0bdb030>] __schedule_bug+0x53/0x61
[  355.760771]  [<c0be6208>] __schedule+0x60/0x5b8
[  355.760778]  [<c0bdb429>] ? printk+0x4d/0x4f
[  355.760785]  [<c0be67f6>] schedule+0x5f/0x61
[  355.760790]  [<c043e5c0>] do_exit+0xe5/0x7de
[  355.760797]  [<c0bdb429>] ? printk+0x4d/0x4f
[  355.760804]  [<c043c951>] ? print_oops_end_marker+0x2f/0x31
[  355.760810]  [<c0bea294>] oops_end+0x98/0x9e
[  355.760816]  [<c0bda845>] no_context+0x17c/0x184
[  355.760822]  [<c0bdb401>] ? printk+0x25/0x4f
[  355.760829]  [<c0bda96f>] __bad_area_nosemaphore+0x122/0x12a
[  355.760835]  [<c0bda98e>] bad_area_nosemaphore+0x17/0x19
[  355.760842]  [<c0bec12a>] __do_page_fault+0x32c/0x3ac
[  355.760850]  [<c047b720>] ? wake_up_klogd+0x34/0x3d
[  355.760856]  [<c047ba51>] ? console_unlock+0x328/0x330
[  355.760862]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.760868]  [<c0bec1b5>] do_page_fault+0xb/0xd
[  355.760874]  [<c0be9bca>] error_code+0x5a/0x60
[  355.760882]  [<c06f007b>] ? cfq_set_request+0x54/0x27e
[  355.760888]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.760894]  [<c0454e4b>] ? kthread_data+0xf/0x13
[  355.760900]  [<c047e313>] ? irq_thread_dtor+0x54/0x9e
[  355.760907]  [<c0452926>] task_work_run+0x68/0x8a
[  355.760912]  [<c043e878>] do_exit+0x39d/0x7de
[  355.760920]  [<c043c951>] ? print_oops_end_marker+0x2f/0x31
[  355.760926]  [<c0bea294>] oops_end+0x98/0x9e
[  355.760932]  [<c0bda845>] no_context+0x17c/0x184
[  355.760939]  [<c0bda96f>] __bad_area_nosemaphore+0x122/0x12a
[  355.760946]  [<c040747b>] ? native_sched_clock+0x46/0x4b
[  355.760952]  [<c0bda98e>] bad_area_nosemaphore+0x17/0x19
[  355.760958]  [<c0bec12a>] __do_page_fault+0x32c/0x3ac
[  355.760965]  [<c06fae84>] ? __delay+0xe/0x10
[  355.760971]  [<c06f597b>] ? plist_del+0x41/0x4c
[  355.760977]  [<c04690e4>] ? dequeue_pushable_task+0x1f/0x45
[  355.760983]  [<c046a46e>] ? dequeue_task_rt+0x27/0x2e
[  355.760989]  [<c045dccc>] ? dequeue_task+0x93/0x9b
[  355.760996]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.761002]  [<c0bec1b5>] do_page_fault+0xb/0xd
[  355.761007]  [<c0be9bca>] error_code+0x5a/0x60
[  355.761014]  [<c0bec1aa>] ? __do_page_fault+0x3ac/0x3ac
[  355.761020]  [<c08eda0a>] ? dwc3_thread_interrupt+0x449/0x5b9
[  355.761027]  [<c046c762>] ? __wake_up+0x40/0x47
[  355.761033]  [<c047daac>] irq_thread_fn+0x18/0x2a
[  355.761039]  [<c047e221>] irq_thread+0x81/0x11f
[  355.761045]  [<c047da94>] ? irq_finalize_oneshot+0x7c/0x7c
[  355.761051]  [<c047e2bf>] ? irq_thread+0x11f/0x11f
[  355.761057]  [<c047e1a0>] ? wake_threads_waitq+0x31/0x31
[  355.761062]  [<c0454997>] kthread+0x87/0x8c
[  355.761070]  [<c0bef237>] ret_from_kernel_thread+0x1b/0x28
[  355.761076]  [<c0454910>] ? __kthread_parkme+0x55/0x55