Hi,
I want to build a module for Sitara Processor SDK 1.00.00.03 on Ubuntu PC. The make error message is as following:
uj@uj-7696:~/Documents/Linux_drv$ make
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- -C /home/u64rj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b M=`pwd` modules -I/home/u64rj/AM335X_StarterWare_02_00_01_01/include/hw
make[1]: Entering directory `/home/u64rj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b'
ERROR: Kernel configuration is invalid.
include/generated/autoconf.h or include/config/auto.conf are missing.
Run 'make oldconfig && make prepare' on kernel src to fix it.
WARNING: Symbol version dump /home/u64rj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b/Module.symvers
is missing; modules will have no dependencies and modversions.
CC [M] /home/u64rj/Documents/Linux_drv/hello_mdvr.o
In file included from <command-line>:0:0:
/home/u64rj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b/include/linux/kconfig.h:4:32: fatal error: generated/autoconf.h: No such file or directory
compilation terminated.
make[2]: *** [/home/u64rj/Documents/Linux_drv/hello_mdvr.o] Error 1
make[1]: *** [_module_/home/u64rj/Documents/Linux_drv] Error 2
make[1]: Leaving directory `/home/u64rj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b'
make: *** [all] Error 2
uj@uj-7696:~/Documents/Linux_drv$ ls -l
total 12
-rw-rw-r-- 1 u64rj u64rj 2939 Sep 22 19:46 hello_mdvr.c
-rw-rw-r-- 1 u64rj u64rj 593 Sep 22 20:25 Makefile
-rw-rw-r-- 1 u64rj u64rj 592 Sep 22 20:23 Makefile~
uj@uj-7696:~/Documents/Linux_drv$
Sitara StarterWare is downloaded and its header file path is included in the Makefile:
#PATH=${PATH}:/home/uj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/linux-devkit/sysroots/i686-arago-linux/usr/bin
obj-m += hello_mdvr.o
INC=-I/home/u64rj/AM335X_StarterWare_02_00_01_01/include/hw
all:
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- -C /home/uj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b M=`pwd` modules $(INC)
clean:
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- -C /home/uj/ti-processor-sdk-linux-am335x-evm-01.00.00.03/board-support/linux-3.14.43+gitAUTOINC+875c69b2c3-g875c69b M=`pwd` clean
There are two header files missing from the error message. How can I fix it?
Thanks,