Other Parts Discussed in Thread: PCF8575
Hello,
I'm currently using EZSDK version 5_05_02_00. Using the following links I was able to make some progress with changing the memory map from the default 1GB to 256MB:
processors.wiki.ti.com/.../EZSDK_Memory_Map
I've made most of the simple changes but have some questions about the memory map. The second link, the wiki, mentions updating the MemSegmentDefinition.xs file as per your new memory map. The wiki provides a sample memory map for 256MB. This memory map doesn't match the MemsegmentDefinition_256MB.xs that comes with the EZSDK. I've pasted the contents of the file below:
function getMemSegmentDefinition(platFormMem)
{
var memory = new Array();
memory[0] = ["VIDEO_M3_VECTOR",
{
name: "VIDEO_M3_VECTOR",
base: 0x0,
len: 0x400,
space: "code"
}];
memory[1] = ["VPSS_M3_VECTOR",
{
name: "VPSS_M3_VECTOR",
base: 0x400,
len: 0x600,
space: "code"
}];
memory[2] = ["DSP",
{
name: "DSP",
base: 0x89500000,
len: 0x00C00000,
space: "code/data"
}];
memory[3] = ["VIDEO_M3_EVENT_BUFFER",
{
name: "VIDEO_M3_EVENT_BUFFER",
base: 0x8D500000,
len: 0x00100000,
space: "data"
}];
memory[4] = ["VIDEO_M3_DATA",
{
name: "VIDEO_M3_DATA",
base: 0x8D600000,
len: 0x00D00000,
space: "data"
}];
memory[5] = ["VIDEO_M3_CODE",
{
name: "VIDEO_M3_CODE",
base: 0x8E300000,
len: 0x00100000,
space: "code"
}];
memory[6] = ["LOGGER_SM",
{
name: "LOGGER_SM",
base: 0x8E400000,
len: 0x00200000,
space: "data"
}];
memory[7] = ["VPSS_M3_EVENT_BUFFER",
{
name: "VPSS_M3_EVENT_BUFFER",
base: 0x8E600000,
len: 0x00100000,
space: "data"
}];
memory[8] = ["VPSS_M3_DATA",
{
name: "VPSS_M3_DATA",
base: 0x8E700000,
len: 0x00E00000,
space: "data"
}];
memory[9] = ["VPSS_M3_CODE",
{
name: "VPSS_M3_CODE",
base: 0x8F500000,
len: 0x00200000,
space: "code"
}];
memory[10] = ["IPC_SR_COMMON",
{
name: "IPC_SR_COMMON",
base: 0x8F700000,
len: 0x00200000,
space: "data"
}];
memory[11] = ["HDVPSS_NOTIFY_MEM",
{
name: "HDVPSS_NOTIFY_MEM",
base: 0xAF900000,
len: 0x00200000,
space: "data"
}];
memory[12] = ["HDVPSS_V4L2_FBDEF_MEM",
{
name: "HDVPSS_V4L2_FBDEF_MEM",
base: 0xAFB00000,
len: 0x00200000,
space: "data"
}];
memory[13] = ["HDVPSS_DESC",
{
name: "HDVPSS_DESC",
base: 0xAFD00000,
len: 0x00200000,
space: "data"
}];
memory[14] = ["MEMCFG_SPACE",
{
name: "MEMCFG_SPACE",
base: 0xAFF00000,
len: 0x000FF000,
space: "data"
}];
memory[15] = ["VIDEO_M3_LOAD_TABLE",
{
name: "VIDEO_M3_LOAD_TABLE",
base: 0xAFFFF000,
len: 0x00000800,
space: "data"
}];
memory[16] = ["VPSS_M3_LOAD_TABLE",
{
name: "VPSS_M3_LOAD_TABLE",
base: 0xAFFFF800,
len: 0x00000800,
space: "data"
}];
return (memory);
}
In addition, the .xs file has more sections that I do not see in the wikipedia page; they overlap with the sections that are reserved for firmware. I also see them in the MemSegmentDefinition.xs file that is used for the 1GB eval board. I'm wondering what some of these sections are, such as VPSS_M3_EVENT_BUFFER, VPSS_M3_DATA, and VPSS_M3_CODE.
I also had questions about the sample memory map. Why is the memory map not contiguous like the 1GB sample? Why are there blocks of inaccessible memory, such as 0x89100000 and 0x8F900000, throughout the memory map?
Lastly, is it ok for the DSP to have no memory for it's code and data sections? The sample memory map provides no memory whereas the MemSegmentDefinition_256MB.xs file provides it 12MBs.
Thanks for any help that can be provided.