Other Parts Discussed in Thread: AM1808, OMAPL138, DA8XX
Hi, I am working with EVM AM1808 , it work well with linux and the mDDR clock is 150MHz.
We have a custom board with the same mDDR and OMAPL138.
If the mDDR clock is 140MHz (SYSCLK1 of PLL1 at 280MHz) the board work well with U-Boot and Linux .
If the mDDR clock is 150MHz (SYSCLK1 of PLL1 at 300MHz) the board work well with U-Boot but Linux does't boot !!!!!
I have checked the time parameter (SDTIMR1,SDTIMR2 registers) and all is goods. With the same value on EVM all is OK.
Can you help me ?