Other Parts Discussed in Thread: DM385
Hi TI,
I'm in customized DM385 platform
I'm working TRISTREAM Full feature Usecase..,
I have two camera's .., I can able to switch between those two but sometimes I'm getting the error log like
[m3vpss ] ##################### REISZER OVERFLOW OCCURED: RESTARTING...############################
[m3vpss ] Iss_csi2 init called !!!!!!
[m3vpss ] ROH: in csi2_init
[m3vpss ] ROH: In csi2_irq_init
[m3vpss ] IN csi2_open
[m3vpss ] IN csi2_reset
[m3vpss ] IN csi2_config
[m3vpss ] IN csi2_config_power
[m3vpss ] IN csi2_config_control
[m3vpss ] IN csi2_config_complexio
[m3vpss ] IN csi2_config_complexio
[m3vpss ] IN csi2_config_timing
[m3vpss ] Iss_Ov5640Enable
[m3vpss ] gOv5640_I2c_ctrl.i2cInstId is 2
[m3vpss ] clear power down
[m3vpss ] Iss_device16AddWrite8
[m3vpss ] I2C2: DEV 0x3c: WR 0x3008 = 0x02
[m3vpss ] IN csi2_wait_phy_reset--->
After that entire links got crashed !!! Why I'm getting the error log ??? What it's denote ???
Any suggestion to solve ???
Regards,
Rajesh Kannan.S