Hi Sivaraj, Do you know if either of these screens will work with the development Kit ?
Beaglebone Black Cape - LCD (7.0") - DEV-12086 - SparkFun Electronics
DEV-12086: The 7.0” resistive touch LCD touch from 4D Systems is a cape specifically designed for the Beaglebone Black, and provides a 7.0” primary display for th
Beaglebone Black Cape - LCD (4.3") - DEV-12085 - SparkFun Electronics
DEV-12085: The 4.3” resistive touch LCD touch from 4D Systems is a cape specifically designed for the Beaglebone Black, and provides a 4.3” primary display for th
I read the connector is Beagle Bone Black, but its not clear which screen is supported and why? screen size / controller etc ?
data sheet for the 7" version here cdn.sparkfun.com/.../4DCAPE-70T_datasheet_R_1_1.pdf
4.3" here cdn.sparkfun.com/.../uLCD-43-PT-AR_datasheet_R_1_4.pdf
I could'nt find the previously recomended LCD7 Lite screen for sale anywhere..
Thanks,
Ben