Other Parts Discussed in Thread: TCI6638K2K, 66AK2H12, 66AK2H14
Hi All,
We are currently using a customized board with K2H14 processor. When we are connecting with the processor through JTAG and loading the GEL File it is showing the error. Can I get any idea regarding this. I am new to this architecture.
C66xx_0: GEL Output:
Connecting Target...
C66xx_0: GEL Output: TCI6638K2K GEL file Ver is 1.3
C66xx_0: GEL Output: Detected PLL bypass enabled: SECCTL[BYPASS] = 0x00800000
C66xx_0: GEL Output: (2a) MAINPLLCTL1 = 0x00000040
C66xx_0: GEL Output: (2b) PLLCTL = 0x00000048
C66xx_0: GEL Output: (2c) PLLCTL = 0x00000048
C66xx_0: GEL Output: (2d) Delay...
C66xx_0: GEL Output: (2e) SECCTL = 0x00810000
C66xx_0: GEL Output: (2f) PLLCTL = 0x0000004A
C66xx_0: GEL Output: (2g) Delay...
C66xx_0: GEL Output: (2h) PLLCTL = 0x00000048
C66xx_0: GEL Output: (4)PLLM[PLLM] = 0x0000000F
C66xx_0: GEL Output: MAINPLLCTL0 = 0x05000000
C66xx_0: GEL Output: (5) MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (5) MAINPLLCTL1 = 0x00000040
C66xx_0: GEL Output: (6) MAINPLLCTL0 = 0x07000000
C66xx_0: GEL Output: (7) SECCTL = 0x00890000
C66xx_0: GEL Output: (8a) Delay...
C66xx_0: GEL Output: PLL1_DIV3 = 0x00008002
C66xx_0: GEL Output: PLL1_DIV4 = 0x00008004
C66xx_0: GEL Output: PLL1_DIV7 = 0x00000000
C66xx_0: GEL Output: (8d/e) Delay...
C66xx_0: GEL Output: (10) Delay...
C66xx_0: GEL Output: (12) Delay...
C66xx_0: GEL Output: (13) SECCTL = 0x00090000
C66xx_0: GEL Output: (Delay...
C66xx_0: GEL Output: (Delay...
C66xx_0: GEL Output: (14) PLLCTL = 0x00000041
C66xx_0: GEL Output: PLL has been configured (CLKIN * PLLM / PLLD / PLLOD = PLLOUT):
C66xx_0: GEL Output: PLL has been configured (122.88 MHz * 16 / 1 / 2 = 983.04 MHz)
C66xx_0: GEL Output: Power on all PSC modules and DSP domains...
C66xx_0: Trouble Reading Register ControlRegisters_DNUM: (Error -1139 @ 0x50) Lost debug connection to device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
C66xx_0: GEL: Error while executing OnTargetConnect(): Target failed to read register ControlRegisters_DNUM at (DNUM==0) [xtcievmk2x.gel:687] at Set_PSC_State(1, 5, 0x3) [xtcievmk2x.gel:908] at Set_Psc_All_On() [xtcievmk2x.gel:636] at Global_Default_Setup_Silent() [xtcievmk2x.gel:565] at OnTargetConnect() .
Can i get the Detailed document of PSC and register description of the K2H14. Can i Get the support from the TI as soon as possible.
Thanks in advance.
Regards,
Avinash N