This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR2 issue while booting



Hi,

I am using two ddr2 with 256*2 = 512MB in my am33xx platform. It is intefraced with EMIF port with Address lines and using D0-D15 for dual ddr2 purpose. I want to use single ddr2 in my existing evm board that mean it should recognize it as 256mb ddr2.

I am removing one ddr2 on my board. is there any issue or any u-boot changes required for recognizing single ddr2 in my processor.

I am using the same u-boot try to run, but it is not booting.

Regard,

Anil