This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have to downgrade a DM8168 SW that runs on both ARM and DSP to L138. What are the things that are different and I need to be care of when porting from DM8168 to L138?
(1) The clock speeds are different;
(2) DM8168 supports SYSBIOS while L138 supports DSPBIOS;
(3) DM8168 supports DDR3 while L138 supports DDR2;
(4) DM8168 has some on chip memory while L138 does not (not sure ?);
What else?
Thanks,
Zhao