This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trouble in using NDK example with EVMDM6437



Hi,

        I am working on  NDK example -the client. Something has confused me for a long time. I have done as what the <Getting Started With the C6000 Network Development Kit.pdf> has told me in the CCS v5 enviroment which  run on the windows XP system .The DSP work well with the UDP.However,it is not on the win7 system.The DSP can not detect  a valid link after I set the IP address on PC manually.The PC is directly connected with the DSP by cable.It is shown like bellow when I debug.The version of NDK is 1.92.

[C64XP_0] TCP/IP Stack Example Client

[C64XP_0] Using MAC Address: 00-09-0e-12-45-34

       The sentence "[C64XP_0] Link Status: 100Mb/s Full Duplex on PHY 0" never appeared on win7,but it does on XP .why?

thank you very much!