This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 SPI0 and UART0 pin multipexing

​Hi 

I have a question about C6747(ZKB) pin multiplexing.
My customer would like to use the SPI0 and UART​0.
But some of these pins are multiplexed.
pin
R3    UART0_RXD 
P3    UART0_TXD 
N4    SPI0_ENA/ UART0_CTS
R5    SPI0_SCS[0]/ UART0_RTS
 T5    SPI0_CLK/
P6    SPI0_SIMO[0]
R6    SPI0_SOMI[0]
 
They don't need the flow control of UART function.
If UART flow control (RTS and CTS) are not used, can we use the UART0 and SPI0 together?
  
Best Regards,
Takahiro Ogo