Other Parts Discussed in Thread: CC1350
Hi,
i am working on a project that uses TIRTOS and the SPI driver on CC1350. Unfortunately this involves 2 SPI devices (a sensor and a eprom) that don't support the same SPI frame format.
One device only supports SPI_POL0_PHA1 and the other only SPI_POL0_PHA0 or SPI_POL1_PHA1.
What is the recommended way to deal with this? Is i possible to use 2 SPI interfaces that are mapped to the same pins, where each would be configured with different frame format? An added complexity is that both devices might be accessed from different tasks.
Or will i have to close and reopen the SPI driver with the different format each time i switch between the two SPI devices?
Thanks