I am using evmk2h with an amc2pcie adapter. EVMK2H is acting as root complex and a xilinx virtex 7 board is acting as endpoint. When I measured the resistance between B14-B15 of PCIe finger on amc2pcie adapter mounted on EVMK2H, it gives me value of 4.6 mega ohms. while resistance between B14-B15 of virtex 7 is 150 ohm. What effect that difference can cause? While I check specs of PCIe it shows both resistances are same. But I couldn't find any reason.
Regards
Rao