We designed a board with 3 DSP´s which we want to connect via the USB interface. But we found a short-circuit between USB_VDDA3P3 and Ground on the first prototype boards. We are able to disconnect this powerlines and use the board in a different way (without USB).
But actual there is still a problem with the C5535. It seems to be that the bootloader doesn´t work anymore. We are able to connect every DSP over a JTAG-Chain and start a simple FW-File with the debugger of CCSV4. But if we program the file to the SPI-ROM nothing happened after a power on reset.
The BIN-file is tested on the ezdspC5535 and worked fine.
The design of each DSP on the prototype boards is similar to the ezdspC5535 design (except USB_VDDA3P3).
We found the note in the datasheet that every USB power supply should connect to ground if it isn´t used. Furthermore the pin USB_VBUS is still connected to 5V.
Is it possible that the bootloader doesn´t work due to the USB interface?
Maybe someone has another idea why the DSP doesn´t load the boot image.
Thanks in advance
Best regards
Marcus