Hi,
I am question about newlib.
The manifest of XDCTools is described as follows.
"several pre-compiled newlib libraries are also provided under the following license"
- XDCTools 3.25.04.88 GA Manifest
software-dl.ti.com/.../xdctools_3_25_04_88_manifest.html
I want to know which library is included newlib.
Because, I do not want to use the newlib to conflict with LGPL.
I think the library that exists under the following folder is included newlib.
C:\ti\xdctools_3_25_04_88\packages\gnu\targets\arm\libs\install-native\arm-none-eabi\lib
Is my thinking correct?
Best regards,
H.U