I am using the code in C:\ti\pdk_C6748_2_0_0_0\C6748_StarterWare_1_20_03_03\examples\lcdkC6748 for my LCDKC6748 device. The purpose of the code is to give Audio In/out from on-board Codec using C6748 DSP.
Since it is not there as a project, I have copied the .c files into an empty SYS/BIOS project. It is giving me following list of errors
#10010 errors encountered during linking; "McASPEcho.out" not built
#10234-D unresolved symbols remain
unresolved symbol EDMA3CIrIntr, first referenced in ./main.obj
unresolved symbol EDMA3EnableTransfer, first referenced in ./main.obj
unresolved symbol EDMA3Init, first referenced in ./main.obj..... and so on.
Any help please.