This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x with 128Mbit NAND flash

Hi,

Hi we need some confirmation about the NAND flash supported by AM335x.
We need to know if AM335x GPMC supports 128Mbit NAND flash "NAND128W3A" (x8 bus)

The TRM mentions "Device from 512Mbit (64MByte)", so do we need to connect
the flash with size 512Mbit or more?
And the "Table 26-14. Supported NAND Devices" mentions the page size as "2048"
but the above flash is only 512+16 Bytes.

Can we assume the above 128Mbit flash is not supported.
Please let us know if there is anything else to be considered when
using a NAND flash for booting.

Best Regards
Kummi