Hi,
Linux can't launch filesystem with NFS by ipstatic. Prompt Linux doesn't appear and this one remains frozen.
Communication with NFS Server is good.
Would you have an idea to resolve this one? Thanks
I put you the starting sequence with uboot settings:
---------------------------------------------------------------------------------------------------------------------------------------------------------------
OMAP-L138 LCDK initialization passed!
Booting TI User Boot Loader
UBL Version: 1.65
UBL Flashtype: NAND
Starting NAND Copy...
Valid magicnum, 0x55424CBB, found in block 0x00000006.
DONE
Jumping to entry point at 0xC1080000.
NAND: 128 MiB
MMC: davinci: 0
Bad block table not found for chip 0
Bad block table not found for chip 0
Bad block table written to 0x000007fe0000, version 0x01
Bad block table written to 0x000007fc0000, version 0x01
In: serial
Out: serial
Err: serial
Net: Working without Ethernet PHY at 100Mb/s
DaVinci-EMAC
Hit any key to stop autoboot: 0
U-Boot >
U-Boot >
U-Boot > pri
autoload=no
baudrate=115200
bootargs=console=ttyS1,115200n8 noinitrd rw mem=32M@0xc0000000 mem=64M@0xc4000000 root=/dev/nfs nfsroot=192.168.1.2:/home/astruc/targetfs,nolock ip=192.168.1.4:192.168.1.2:192.168.1.1:255.255.255.0:astruc::off
bootcmd=tftpboot;bootm
bootdelay=3
bootfile=uImage-cpu4-omapl138.bin
ethact=DaVinci-EMAC
ethaddr=00:00:00:fc:fa:c3
gatewayip=192.168.1.1
ipaddr=192.168.1.4
ipstatic=192.168.1.4:192.168.1.2:192.168.1.1:255.255.255.0:astruc::off
netdev=eth0
netmask=255.255.255.0
nfsroot=192.168.1.2:/home/astruc/targetfs
rootpath=/home/astruc/targetfs
serverip=192.168.1.2
stderr=serial
stdin=serial
stdout=serial
ver=U-Boot 2012.04.01 (Oct 15 2015 - 10:05:38)
Environment size: 722/65532 bytes
U-Boot > tftpboot;bootm
Using DaVinci-EMAC device
TFTP from server 192.168.1.2; our IP address is 192.168.1.4
Filename 'uImage-cpu4-omapl138.bin'.
Load address: 0xc0700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
################
done
Bytes transferred = 2408832 (24c180 hex)
## Booting kernel from Legacy Image at c0700000 ...
Image Name: Linux-3.3.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2408768 Bytes = 2.3 MiB
Load Address: c0008000
Entry Point: c0008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0
Linux version 3.3.0 (astruc@ubuntu) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 PREEMPT Thu Oct 15 15:39:24 CEST 2015
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction cache
Machine: AM18x/OMAP-L138 lcdk board
Memory policy: ECC disabled, Data cache writeback
BUG: mapping for 0x80000000 at 0xfffe0000 out of vmalloc space
DaVinci da850/omap-l138/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 24320
Kernel command line: console=ttyS1,115200n8 noinitrd rw mem=32M@0xc0000000 mem=64M@0xc4000000 root=/dev/nfs nfsroot=192.168.1.2:/home/astruc/targetfs,nolock ip=192.168.1.4:192.168.1.2:192.168.1.1:255.255.255.0:astruc::off
PID hash table entries: 512 (order: -1, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 32MB 64MB = 96MB total
Memory: 92320k/92320k available, 5984k reserved, 0K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
vmalloc : 0xc8800000 - 0xff000000 ( 872 MB)
lowmem : 0xc0000000 - 0xc8000000 ( 128 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc0477000 (4540 kB)
.init : 0xc0477000 - 0xc04a1000 ( 168 kB)
.data : 0xc04a2000 - 0xc04d1f80 ( 192 kB)
.bss : 0xc04d1fa4 - 0xc04f392c ( 135 kB)
SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:245
Console: colour dummy device 80x30
Calibrating delay loop... 148.88 BogoMIPS (lpj=744448)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
Setting up static identity map for 0xc0366350 - 0xc03663a8
gpiochip_add: registered GPIOs 0 to 31 on device: DaVinci
gpiochip_add: registered GPIOs 32 to 63 on device: DaVinci
gpiochip_add: registered GPIOs 64 to 95 on device: DaVinci
gpiochip_add: registered GPIOs 96 to 127 on device: DaVinci
gpiochip_add: registered GPIOs 128 to 143 on device: DaVinci
DaVinci: 144 gpio irqs
print_constraints: dummy:
NET: Registered protocol family 16
EMAC: MII PHY configured
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c-gpio i2c-gpio.1: using pins 20 (SDA) and 21 (SCL)
Advanced Linux Sound Architecture Driver Version 1.0.24.
Switching to clocksource timer0_1
musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 180
io scheduler noop registered (default)
da8xx_lcdc da8xx_lcdc.0: GLCD: Found VGA_Monitor panel
Console: switching to colour frame buffer device 80x30
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25) is a AR7
serial8250.0: ttyS1 at MMIO 0x1d0c000 (irq = 53) is a AR7
console [ttyS1] enabled
serial8250.0: ttyS2 at MMIO 0x1d0d000 (irq = 61) is a AR7
brd: module loaded
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xa1 (Micron NAND 128MiB 1,8V 8-bit)
Bad block table not found for chip 0
Bad block table not found for chip 0
Scanning device for bad blocks
Bad block table written to 0x000007fe0000, version 0x01
Bad block table written to 0x000007fc0000, version 0x01
Creating 4 MTD partitions on "davinci_nand.1":
0x000000000000-0x000000020000 : "u-boot env"
0x000000020000-0x0000000a0000 : "u-boot"
0x0000000a0000-0x0000002a0000 : "kernel"
0x0000002a0000-0x000008000000 : "filesystem"
davinci_nand davinci_nand.1: controller rev. 2.5
Fixed MDIO Bus: probed
davinci_mdio davinci_mdio.0: davinci mdio revision 1.5
davinci_mdio davinci_mdio.0: no live phy, scanning all
davinci_mdio: probe of davinci_mdio.0 failed with error -5
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
input: gpio-keys-polled as /devices/platform/gpio-keys-polled.0/input/input0
omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0
omap_rtc: RTC power up reset detected
omap_rtc: already running
i2c /dev entries driver
watchdog watchdog: heartbeat 60 sec
cpuidle: using governor ladder
cpuidle: using governor menu
davinci_mmc davinci_mmc.0: Using DMA, 4-bit mode
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
soc-audio soc-audio.0: ASoC: Failed to create card debugfs directory
ALSA device list:
No soundcards found.
TCP cubic registered
NET: Registered protocol family 17
console [netcon0] enabled
netconsole: network logging started
davinci_emac davinci_emac.1: using random MAC addr: c6:44:4f:1d:d7:78
omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
net eth0: no phy, defaulting to 100/full
IP-Config: Complete:
device=eth0, addr=192.168.1.4, mask=255.255.255.0, gw=192.168.1.1,
host=astruc, domain=, nis-domain=(none),
bootserver=192.168.1.2, rootserver=192.168.1.2, rootpath=
VFS: Mounted root (nfs filesystem) on device 0:13.
Freeing init memory: 168K
INIT: version 2.88 booting
Starting udev
Starting Bootlog daemon: bootlogd.
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1686: No soundcards found...
NOT configuring network interfaces: / is an NFS mount
Wed Nov 6 04:32:00 UTC 2013
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting telnet daemon.
Starting syslogd/klogd: NET: Registered protocol family 10
done
Starting thttpd.
Stopping Bootlog daemon: bootlogd.