Other Parts Discussed in Thread: 66AK2E05
Hi community,
Im working on 66AK2E05 EVM. I burned the re-compiled uboot and skern on 5 EVM and they are booting successfully on NOR Flash. Im using `uboot.bin` file.
With same uboot and skern the other 2 EVM not boot. these boards is freeze when starting, last print is sometimes NAND, sometimes Net, sometimes nothing printed. I checked the Nor flash, and read/write test is OK.
So i decided to boot from Nand, but i cant compile uboot for nand gph image. This is my instructions:
1-make distclean O=~/K2/Uboot/outputs ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
2-make k2e_evm_config O=~/K2/Uboot/outputs ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
3-make k2e_evm_config O=~/K2/Uboot/outputs ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
4-make u-boot-nand.gph O=~/K2/Uboot/outputs ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
Compiler Error is `make: *** No rule to make target `u-boot-nand.gph'. Stop.` .I tried for `u-boot-spi.gph` and got same error.
How can i compile uboot for nand image?
Best Regards,
Srt