This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[OMAP-L138, EMIF] Output Load Capacitance for EMIF

Hello,

My customer wants to confirm whether Output Load Capacitance (Known as CL) specification for EMIF is available or not. 
From the datasheet, It seems it is typically 3 pF, but they are wondering it might be a number for a each pin.

Do you have a CL spec especially for EMIF or do you have a reasonable/suggested number for that ?
They are planing to connect some memories and other devices such as LCD to EMIF and concerned that the output load capacitance requirements are met.

Best Regards,
Naoki kawada