Other Parts Discussed in Thread: AM3352
My customer has the following questions:
I have a question on depopulating the RTC crystal on the AM3352
According to the AM335x Schematic Checklist
If RTC internal oscillator is not used...
This can be the case when:
A 1.8 volt LVCMOS clock source is used rather than a crystal circuit
Connect the clock source to the RTC_XTALIN terminal, leave the RTC_XTALOUT terminal open-circuit, and connect VSS_RTC to VSS if using the ZCZ package option
The AM335x RTC is not used
Leave the RTC_XTALIN and RTC_XTALOUT terminals open-circuit, and connect VSS_RTC to VSS if using the ZCZ package option
Is there a typo in “connect VSS_RTC to VSS” because it already is, both are ground connections.
- Does the VDDS_RTC pin need to be connected to VSS_RTC and VSS?
- Or does power need to be kept on the VDDS_RTC pin?
- Or does the VDDS_RTC pin need to be left floating?