Other Parts Discussed in Thread: OMAP-L138
Hello
I'm trying to setup nested interrupts on the OMAP L138 ARM processor and am unable to successfully do so. I'm doing this within the linux kernel v3.3 and am unsure of what is going wrong. I have attached a modified AINTC initialization module file from the kernel. My modifications are an attempt to follow the instructions listed in the OMAP-L138 DSP+ARM Technical Reference Manual section 12.3.7 - method #2.
I'm looking for help to figure out what I'm doing wrong, in addition to any examples of nested interrupts on the OMAP (any platform really - not just linux). This other e2e question is a year old, so maybe there have been some more examples since then?
Thanks for you time.
Austin
/*
* TI Common Platform Interrupt Controller (cp_intc) driver
*
* Author: Steve Chen <schen@mvista.com>
* Copyright (C) 2008-2009, MontaVista Software, Inc. <source@mvista.com>
*
* This file is licensed under the terms of the GNU General Public License
* version 2. This program is licensed "as is" without any warranty of any
* kind, whether express or implied.
*/
#include <linux/init.h>
#include <linux/irq.h>
#include <linux/io.h>
#include <mach/common.h>
#include <mach/cp_intc.h>
#define STACK_MAX 32
struct Stack {
int data[STACK_MAX];
int size;
};
struct Stack m_nestStack;
void stackInit(struct Stack *stack) {
stack->size = 0;
}
int stackTop(struct Stack *stack) {
if (stack->size == 0)
return -1;
return stack->data[stack->size-1];
}
void stackPush(struct Stack *stack, int d) {
if (stack->size < STACK_MAX)
stack->data[stack->size++] = d;
else
pr_warning("CP_INTC: Nest stack filled\n");
}
void stackPop(struct Stack *stack) {
if (stack->size == 0)
pr_warning("CP_INTC: Nest stack empty\n");
else
stack->size--;
}
static inline unsigned int cp_intc_read(unsigned offset)
{
return __raw_readl(davinci_intc_base + offset);
}
static inline void cp_intc_write(unsigned long value, unsigned offset)
{
__raw_writel(value, davinci_intc_base + offset);
}
/* Disable interrupt */
static void cp_intc_mask_irq(struct irq_data *d)
{
/* XXX don't know why we need to disable nIRQ here... */
cp_intc_write(1, CP_INTC_HOST_ENABLE_IDX_CLR);
cp_intc_write(d->irq, CP_INTC_SYS_ENABLE_IDX_CLR);
cp_intc_write(1, CP_INTC_HOST_ENABLE_IDX_SET);
}
/* Enable interrupt */
static void cp_intc_unmask_irq(struct irq_data *d)
{
cp_intc_write(d->irq, CP_INTC_SYS_ENABLE_IDX_SET);
}
static void cp_intc_ack_irq(struct irq_data *d)
{
cp_intc_write(d->irq, CP_INTC_SYS_STAT_IDX_CLR);
cp_intc_unmask_irq(d);//todo ajr: added
}
static int cp_intc_set_irq_type(struct irq_data *d, unsigned int flow_type)
{
unsigned reg = BIT_WORD(d->irq);
unsigned mask = BIT_MASK(d->irq);
unsigned polarity = cp_intc_read(CP_INTC_SYS_POLARITY(reg));
unsigned type = cp_intc_read(CP_INTC_SYS_TYPE(reg));
switch (flow_type) {
case IRQ_TYPE_EDGE_RISING:
polarity |= mask;
type |= mask;
break;
case IRQ_TYPE_EDGE_FALLING:
polarity &= ~mask;
type |= mask;
break;
case IRQ_TYPE_LEVEL_HIGH:
polarity |= mask;
type &= ~mask;
break;
case IRQ_TYPE_LEVEL_LOW:
polarity &= ~mask;
type &= ~mask;
break;
default:
return -EINVAL;
}
cp_intc_write(polarity, CP_INTC_SYS_POLARITY(reg));
cp_intc_write(type, CP_INTC_SYS_TYPE(reg));
return 0;
}
/*
* Faking this allows us to to work with suspend functions of
* generic drivers which call {enable|disable}_irq_wake for
* wake up interrupt sources (eg RTC on DA850).
*/
static int cp_intc_set_wake(struct irq_data *d, unsigned int on)
{
return 0;
}
static struct irq_chip cp_intc_irq_chip = {
.name = "cp_intc",
.irq_ack = cp_intc_ack_irq,
.irq_mask = cp_intc_mask_irq,
.irq_unmask = cp_intc_unmask_irq,
.irq_set_type = cp_intc_set_irq_type,
.irq_set_wake = cp_intc_set_wake,
};
static void cp_intc_set_nested_level(unsigned int irq, unsigned int level)
{
cp_intc_write((BIT(31) | level), CP_INTC_HOST_NESTING_LEVEL(irq));
}
static int cp_intc_get_nested_level(unsigned int irq)
{
return cp_intc_read(CP_INTC_HOST_NESTING_LEVEL(irq));
}
void cp_intc_irq_handler(unsigned int irq, struct irq_desc *desc)
{
int currLevel;
//1. Mask interrupt
cp_intc_mask_irq(&desc->irq_data);
//2. Obtain current nested level
currLevel = cp_intc_get_nested_level(irq);
//3. Save to the stack
stackPush(&m_nestStack, currLevel);
//4. Set the new level
cp_intc_set_nested_level(irq, davinci_soc_info.intc_irq_prios[irq]);
//5. skip for now...
//6 - 8 handled generically
handle_edge_irq(irq, desc);
//9. Mask interrupt
cp_intc_mask_irq(&desc->irq_data);
//10. Restore priority
currLevel = stackTop(&m_nestStack);
stackPop(&m_nestStack);
//11. Exit
cp_intc_unmask_irq(&desc->irq_data);
}
void __init cp_intc_init(void)
{
unsigned long num_irq = davinci_soc_info.intc_irq_num;
u8 *irq_prio = davinci_soc_info.intc_irq_prios;
u32 *host_map = davinci_soc_info.intc_host_map;
unsigned num_reg = BITS_TO_LONGS(num_irq);
int i;
davinci_intc_type = DAVINCI_INTC_TYPE_CP_INTC;
davinci_intc_base = ioremap(davinci_soc_info.intc_base, SZ_8K);
if (WARN_ON(!davinci_intc_base))
return;
cp_intc_write(0, CP_INTC_GLOBAL_ENABLE);
/* Disable all host interrupts */
cp_intc_write(0, CP_INTC_HOST_ENABLE(0));
/* Disable system interrupts */
for (i = 0; i < num_reg; i++)
cp_intc_write(~0, CP_INTC_SYS_ENABLE_CLR(i));
cp_intc_write(0x4, CP_INTC_CTRL);
cp_intc_write(0, CP_INTC_HOST_CTRL);
/* Clear system interrupt status */
for (i = 0; i < num_reg; i++)
cp_intc_write(~0, CP_INTC_SYS_STAT_CLR(i));
/* Enable nIRQ (what about nFIQ?) */
cp_intc_write(1, CP_INTC_HOST_ENABLE_IDX_SET);
/*
* Priority is determined by host channel: lower channel number has
* higher priority i.e. channel 0 has highest priority and channel 31
* had the lowest priority.
*/
num_reg = (num_irq + 3) >> 2; /* 4 channels per register */
if (irq_prio) {
unsigned j, k;
u32 val;
for (k = i = 0; i < num_reg; i++) {
for (val = j = 0; j < 4; j++, k++) {
val >>= 8;
if (k < num_irq)
val |= irq_prio[k] << 24;
}
cp_intc_write(val, CP_INTC_CHAN_MAP(i));
}
} else {
/*
* Default everything to channel 15 if priority not specified.
* Note that channel 0-1 are mapped to nFIQ and channels 2-31
* are mapped to nIRQ.
*/
for (i = 0; i < num_reg; i++)
cp_intc_write(0x0f0f0f0f, CP_INTC_CHAN_MAP(i));
}
if (host_map)
for (i = 0; host_map[i] != -1; i++)
cp_intc_write(host_map[i], CP_INTC_HOST_MAP(i));
/* Set up genirq dispatching for cp_intc */
for (i = 0; i < num_irq; i++) {
irq_set_chip(i, &cp_intc_irq_chip);
set_irq_flags(i, IRQF_VALID | IRQF_PROBE);
irq_set_handler(i, cp_intc_irq_handler);
}
stackInit(&m_nestStack);
stackPush(&m_nestStack, 31);
/* Enable global interrupt */
cp_intc_write(1, CP_INTC_GLOBAL_ENABLE);
}