This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sendding doorbell by c6678 srio delay 720 ms

Hi all,

         Sometime,Sendding doorbell by c6678 srio will delay 720 ms .My sdk is pdk_c6678_1_1_2_5.I set 1x and speed is 3.125g.Can you tell me why?Thanks.

  • Hi,

    In doorbell interrupt delay case, Are you getting other errors identified too, i.e. SPn_ERR_STAT, ERR_DET, SPn_ERR_DET?

    Better to use the latest PDK version SRIO driver and example for your testing(pdk_C6678_1_1_2_6). Please download the latest MCSDK 2.x for Keystone I devices(C6657/70/78) and the follow user guide here.

    Thanks,

  • Hi Ganapathi,

      Thanks for your reply.

      I use pdk_C6678_1_1_2_6 to test.It is the same .The  value of SPn_ERR_STAT, ERR_DET, SPn_ERR_DET  at normal state  is same with delay state.DoorBell Delay ,Because the LSU context Bit of LSU_STAT_REG is not equal with LSU6 Bit.So it is block .Why is it block?Can you tell me?

    Thanks,

    Best Regards,

    Tory