Other Parts Discussed in Thread: TMS320C6657
Hello,
I'm working with the evaluation kit TMS320C6657 and I need to communicate with A2D through SPI component.
As I read, there is software API in PDK for hardware components and example codes for some of them in BIOS_MCSDK_2.0_User_Guide(UART GPIO etc.) .
In addition I understand that the SPI is connected to the NOR flash memory and to the FPGA on the board, Is there any option to work with it directly through the DSP ?
Is there any example program/codes for the SPI component ?
Thank you,
Joni Sheingouz.