Other Parts Discussed in Thread: AM3352
Hi,
The HW is configured to have 1 USB host and 1 USB device
commands to set USB:
modprobe g_serial modprobe usbserial vendor=0x0525 product=0xa4a7
These two USB I/F are connected together for simple EMI test purpose.
Once I try to send text payload from ttyGS0 to ttyUSB0. like:
echo ddddd > /dev/ttyGS0 /flash # echo ddddd > /dev/ttyGS0 /flash # echo ddddd > /dev/ttyGS0 /flash # tail /dev/ttyUSB0
I will get crash message like:
[ 58.150830] WARNING: CPU: 0 PID: 895 at /opt/pack/linux-3.14.26-g2489c02/drivers/usb/musb/musb_host.c:128 musb_h_tx_flush_fifo+0x60/0x98() [ 58.163885] Could not flush host TX2 fifo: csr: 2103 [ 58.169100] Modules linked in: usbserial usb_f_acm u_serial g_serial libcomposite c_can_platform c_can can_dev [ 58.179718] CPU: 0 PID: 895 Comm: tail Not tainted 3.14.26 #1 [ 58.185754] Backtrace: [ 58.188386] [<c0010d8c>] (dump_backtrace) from [<c0010f28>] (show_stack+0x18/0x1c) [ 58.196336] r6:c06666b2 r5:00000009 r4:c7215bd0 r3:b4eb9ef5 [ 58.202357] [<c0010f10>] (show_stack) from [<c04ca368>] (dump_stack+0x20/0x28) [ 58.209978] [<c04ca348>] (dump_stack) from [<c00350e8>] (warn_slowpath_common+0x6c/0x8c) [ 58.218498] [<c003507c>] (warn_slowpath_common) from [<c00351ac>] (warn_slowpath_fmt+0x38/0x40) [ 58.227630] r8:c06fd408 r7:c745847c r6:00000000 r5:00002103 r4:c8874c12 [ 58.234751] [<c0035178>] (warn_slowpath_fmt) from [<c03605b0>] (musb_h_tx_flush_fifo+0x60/0x98) [ 58.243883] r3:00000002 r2:c06666f0 [ 58.247683] [<c0360550>] (musb_h_tx_flush_fifo) from [<c0361998>] (musb_cleanup_urb+0x58/0xa0) [ 58.256723] r8:00000001 r7:c71ade00 r6:00000000 r5:c745847c r4:c8874c10 [ 58.263839] [<c0361940>] (musb_cleanup_urb) from [<c0361adc>] (musb_urb_dequeue+0xfc/0x144) [ 58.272607] r7:c0008200 r6:a0000013 r5:c71ade00 r4:c715b980 [ 58.278620] [<c03619e0>] (musb_urb_dequeue) from [<c033ba10>] (unlink1+0xe8/0xf4) [ 58.286476] r10:c75026c8 r9:00000000 r8:fffffffe r7:fffffffe r6:60000013 r5:c71ade00 [ 58.294761] r4:c7430400 r3:c03619e0 [ 58.298558] [<c033b928>] (unlink1) from [<c033cf54>] (usb_hcd_unlink_urb+0x94/0xb0) [ 58.306596] r8:00000010 r7:fffffffe r6:60000013 r5:c71ade00 r4:00000000 r3:c732e000 [ 58.314812] [<c033cec0>] (usb_hcd_unlink_urb) from [<c033e0c8>] (usb_kill_urb+0x54/0xcc) [ 58.323307] r7:c75026c0 r6:c7278000 r5:c71ade0c r4:c71ade00 [ 58.329381] [<c033e074>] (usb_kill_urb) from [<bf039530>] (usb_serial_generic_close+0x24/0x98 [usbserial]) [ 58.339517] r6:c7278000 r5:c750cc84 r4:c750cc00 [ 58.344466] [<bf03950c>] (usb_serial_generic_close [usbserial]) from [<bf03702c>] (serial_port_shutdown+0x2c/0x30 [usbserial]) [ 58.356422] r5:c750cc84 r4:c750cc04 [ 58.360243] [<bf037000>] (serial_port_shutdown [usbserial]) from [<c02c9d90>] (tty_port_shutdown+0x80/0x8c) [ 58.370491] [<c02c9d10>] (tty_port_shutdown) from [<c02caa70>] (tty_port_close+0x2c/0x60) [ 58.379076] r6:00000000 r5:c750cc04 r4:c7278000 r3:00000000 [ 58.385106] [<c02caa44>] (tty_port_close) from [<bf0376b0>] (serial_close+0x24/0x28 [usbserial]) [ 58.394328] r5:00000000 r4:c7278000 [ 58.398159] [<bf03768c>] (serial_close [usbserial]) from [<c02c2290>] (tty_release+0x130/0x528) [ 58.407332] [<c02c2160>] (tty_release) from [<c00d05f8>] (__fput+0xe0/0x220) [ 58.414734] r10:c75026c8 r9:00000000 r8:00000010 r7:c7129ad0 r6:c701f150 r5:c69db210 [ 58.423019] r4:c75026c0 [ 58.425717] [<c00d0518>] (__fput) from [<c00d078c>] (____fput+0x10/0x14) [ 58.432754] r10:00000008 r9:c7215ed0 r8:c74bc7f4 r7:00000001 r6:c07170d8 r5:00000000 [ 58.441038] r4:c709f000 [ 58.443749] [<c00d077c>] (____fput) from [<c004d328>] (task_work_run+0x94/0xa8) [ 58.451453] [<c004d294>] (task_work_run) from [<c0036b40>] (do_exit+0x320/0x864) [ 58.459219] r6:00000000 r5:c74bc7c0 r4:c709f000 r3:00000000 [ 58.465233] [<c0036820>] (do_exit) from [<c0037218>] (do_group_exit+0xb0/0xec) [ 58.472816] r7:c74fe624 [ 58.475529] [<c0037168>] (do_group_exit) from [<c0042bc4>] (get_signal_to_deliver+0x4d8/0x548) [ 58.484570] r6:c7215ee4 r5:00000009 r4:c7214000 r3:00418004 [ 58.490583] [<c00426ec>] (get_signal_to_deliver) from [<c04c7468>] (do_signal+0xb0/0x3d0) [ 58.499169] r10:b6f041c8 r9:c7214000 r8:b6f041cc r7:fffffe00 r6:c7214000 r5:00000001 [ 58.507453] r4:c7215fb0 [ 58.510147] [<c04c73b8>] (do_signal) from [<c0010984>] (do_work_pending+0x5c/0xac) [ 58.518095] r10:00000000 r8:c000e4a4 r7:00000003 r6:c000e4a4 r5:c7215fb0 r4:c7214000 [ 58.526405] [<c0010928>] (do_work_pending) from [<c000e360>] (work_pending+0xc/0x20) [ 58.534535] r6:01cfe02d r5:00000003 r4:0007ad90 r3:01cfe02d [ 58.540528] ---[ end trace 6d8a347ab86f198c ]---
what's the problem?