This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there any codec that implements H264 main profile for Omap-l138?

Other Parts Discussed in Thread: OMAP-L138

Hi,

currently I am using DVSDK to develop my application which implements getting H264 main profile from IP camera on ARM side and real-time decoding on DSP side. There is already a codec directory named "codecs-omapl138_4_02_00_00" in DVSDK, but the codec for H264 decoder is base on baseline profile. So:

1. Is there any shared codec for H264 main profile provided from TI?

2. If it cannot be provided, can you tell me how to implement my application for H264 main profile decoding? Is it reasonable to rewrite some kind of h264 open library (e.g. x264) and intergrate into a self-defined codec?

 

Thank you very much!