This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

timing for 320x240 LCD

Guru 20755 points

Hello,

I have difficulties finding the correct timing for 320x240 display (QVGA).

For other resolutions it is very easily can be found, but not for these one.

echo 148500,1920/88/148/44,1080/4/36/5,1 > /sys/devices/platform/vpss/display0/timings

Can anyone please help ?

Regards,

Ran

  • Hello,

    Below are the timing parameters for the different CEA and VESA modes.

    echo 25200,640/16/48/96,480/10/33/2,1 > /sys/devices/platform/vpss/display0/timings
    echo 74250,1280/440/220/40,720/5/20/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 74250,1280/110/220/40,720/5/20/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 27027,720/16/60/62,480/9/30/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 108000,2880/48/272/256,576/5/39/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 27027,1440/38/114/124,240/4/15/3,1 > /sys/devices/platform/vpss/display0/timings
    echo 27000,1440/24/138/126,288/2/19/3,1 > /sys/devices/platform/vpss/display0/timings
    echo 74250,1920/528/148/44,540/2/15/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 74250,1920/88/148/44,540/2/15/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 148500,1920/88/148/44,1080/4/36/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 27000,720/12/68/64,576/5/39/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 54000,1440/24/136/128,576/5/39/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 148500,1920/528/148/44,1080/4/36/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 108108,2880/64/240/248,480/9/30/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 74250,1920/638/148/44,1080/4/36/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 25175,640/16/48/96,480/11/31/2,1 > /sys/devices/platform/vpss/display0/timings
    echo 40000,800/40/88/128,600/1/23/4,1 > /sys/devices/platform/vpss/display0/timings
    echo 33750,848/16/112/112,480/6/23/8,1 > /sys/devices/platform/vpss/display0/timings
    echo 79500,1280/64/192/128,768/3/20/7,1 > /sys/devices/platform/vpss/display0/timings
    echo 83500,1280/72/200/128,800/3/22/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 85500,1360/64/256/112,768/3/18/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 108000,1280/96/312/112,960/1/36/3,1 > /sys/devices/platform/vpss/display0/timings
    echo 108000,1280/48/248/112,1024/1/38/3,1 > /sys/devices/platform/vpss/display0/timings
    echo 65000,1024/24/160/136,768/3/29/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 121750,1400/88/232/144,1050/3/32/4,1 > /sys/devices/platform/vpss/display0/timings
    echo 106500,1440/80/232/152,900/3/25/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 146250,1680/104/280/176,1050/3/30/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 85500,1366/70/213/143,768/3/24/3,1 > /sys/devices/platform/vpss/display0/timings
    echo 148500,1920/88/80/44,1080/4/36/5,1 > /sys/devices/platform/vpss/display0/timings
    echo 68250,1280/48/80/32,768/3/12/7,1 > /sys/devices/platform/vpss/display0/timings
    echo 101000,1400/48/80/32,1050/3/23/4,1 > /sys/devices/platform/vpss/display0/timings
    echo 119000,1680/48/80/32,1050/3/21/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 79500,1280/48/80/32,800/3/14/6,1 > /sys/devices/platform/vpss/display0/timings
    echo 74250,1280/110/220/40,720/5/20/5,1 > /sys/devices/platform/vpss/display0/timings

    BR

    Margarita

  • Hi Margarita,

    Thank you very much,
    But I can't see in the list the 320x240 60hz LCD resolution.

    Regards,
    Ran
  • Hello,

    Check this topic :
    e2e.ti.com/.../300932

    BR
    Margarita