Other Parts Discussed in Thread: TMS320C6678, 66AK2H14
Hello All,
we have made a customized board with Quad Processor Board (three TMS320C6678 + One 66AK2H14). In our JTAG Chain 66AK2H14 is the first processor followed by three TMS320C6678 processor.
We have Bypassed the 66AK2H14 from the JTAG chain and we have tested the other three TMS320C6678 processor.
We can able to run the GEL file(Successfully Initialized) and we can able to test the Three TMS320C6678.
We have tested in Two Scenario,
1. We have bypassed the three TMS320C6678 and we trying to test the
66AK2H14 processor alone.
2. We have all the four processor in the tool chain and we trying to test the 66AK2H14 processor.
We are currently using the ..\..\emulation\boards\xtcievmk2x\gel\xtcievmk2x.gel for Initial test process.
In our customized board and In EVMK2HX the core clock is 122.88MHz
Question's:
1. What is the No Boot Configuration value?
2. We are trying to Load the EVM GEL file and test. In the GEL File till the core clock we can able to access once entering the PCS section (Set_Psc_All_On()). It is showing Error as,
C66xx_0: Trouble Reading Memory Block at 0x2350814 on Page 0 of Length 0x4: (Error -1139 @ 0x2350814) Lost debug connection to device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)
C66xx_0: GEL: Error while executing OnTargetConnect(): Target failed to read 0x02350814 at (*(mdstat)&0x1f) [xtcievmk2x - K2H14.gel:694] at Set_PSC_State(1, 5, 0x3) [xtcievmk2x - K2H14.gel:908] at Set_Psc_All_On() [xtcievmk2x - K2H14.gel:636] at Global_Default_Setup_Silent() [xtcievmk2x - K2H14.gel:565] at OnTargetConnect() .