This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
FFTLIB supports real and complex inputs. Please refer below Link to download.
in the description it says that the library is suitable for the following devices:
66AK2E02 66AK2E05 66AK2H06 66AK2H12
TMS320C6670 TMS320C6671 TMS320C6672 TMS320C6674 TMS320C6678
Library can be used on the C6657 ?
How can i know the FFT computational time for different points to this Keystone multicore DSP?Anybody knows how to get the benchmarks related to FFT ?
Hi !
I would need a real2complex-FFT and a complex2real-IFFT for 32bit-FIXPOINT with in IN-PLACE-Transformation for C66x. Is it content of any library ?
If not could I get the Assembler-sources of the following functions ?
void DSP_fft32x32 (
const int * restrict ptr_w,
int npoints,
int * restrict ptr_x,
int * restrict ptr_y
);
void DSP_ifft32x32 (
const int * restrict ptr_w,
int npoints,
int * restrict ptr_x,
int * restrict ptr_y
);